STM32H747 Touchgfx Custom Board Config
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2023-12-02 5:44 PM
hi .
I am trying to use a display lcd using parallel rgb (LTDC RGB888) with STM32h747XIH on a special board.
STM32CUBE-IDE v1.14.0
Touchgfx Designer v4.22.1
STM32Cube_FW_H7_V1.11.1
My project creation steps are as follows :
1-Stm32 project creation
2-RCC Setting HSE & LSE
3- I open the LTDC unit and select "Display type RGB888(24 bits)". DSIHOST is automatically checked but DSIHOST Disable is selected.if I try to remove the DSI host tick, CubeIde Message "DSIHOST, LTDC are linked,both configurations will be lost would you like to continue anyway ?" and
 4-Middleware and Software Packs -> X-CUBE-TOUCHGFX -> Graphics Aplication checked
 5 -Middleware and Software Packs -> FreeRtos -CMSIS_v2
6- Save and generate code
7-Touchgfx->ApplicationTemplate.touchgfx.part duble click and touchgfx designer opening .click Generate code
and fail :
Post Generate Target
touchgfx update_project
Unable to locate C:/Users/sinan/STM32CubeIDE/workspace_1.14.0/sdsd/.cproject
Failed
Yeah, there's really no such file there.
if I copy cm7/cproject from a subfolder here, a lot of different error messages appear.
here's no solution for me .
Then I proceed to the 2nd method. I create the project using the STM32h747 example in the touchgfx designer
Then i change the LTDC unit to RGB888 24 bit ,DSIHOST Disable
Failed !
../../Drivers/STM32H7xx_HAL_Driver/Inc/stm32h7xx_hal_ltdc_ex.h:32:10: fatal error: stm32h7xx_hal_dsi.h: No such file or directory
I want to generate code with the 1st method.
by adding a blank project with the necessary peripheral settings and touchgfx
What am I doing wrong?
Can you help me?
Thanks
Solved! Go to Solution.
- Labels:
-
STM32CubeIDE
Accepted Solutions
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2024-04-05 12:57 AM
Problem is solved. There is no need to turn off the DSI host. Start the DSI host in "command mode via apb interface"
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2023-12-06 3:51 PM
The first problem is solved.
But it still keeps giving the following error in cubeide when turned on in ltdc parallel rgb mode.
../../Drivers/STM32H7xx_HAL_Driver/Inc/stm32h7xx_hal_ltdc_ex.h:32:10: fatal error: stm32h7xx_hal_dsi.h: No such file or directory
The solution to the first problem is to create the project completely in cubemx. Uncheck "Generate Under Root" before pressing the generate code button in cubemx.
If I continue with my original question, why can't it find the dsi.h library ? how i fix it ?
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2024-04-04 10:51 PM
I've came across the same problem. Disabling DSI mode via "project_name.ioc", "stm32h7xx_hal_dsi.h" file is not included in project workspace but It seems compiler try to execute this line even DSI mode is not active.
Then I realized there is a code in "stm32h7xx_hal_ltdc_ex.h" file at line 32. "stm32h7xx_hal_ltdc_ex.h" file cannot be reached by stm32cubide workspace but can be manually reached "..\Drivers\STM32H7xx_HAL_Driver\Inc" directory.
I tried to comment out #include "stm32h7xx_hal_dsi.h" line and all function prototypes in "stm32h7xx_hal_ltdc_ex.h" file and build the project "No such file or directory" error no longer exist.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2024-04-05 12:57 AM
Problem is solved. There is no need to turn off the DSI host. Start the DSI host in "command mode via apb interface"