2021-09-28 06:19 PM
Hi Guys,
I am in the mist of changing my linker file as I just recently found out that my DMA buffers are located in 0x2001FF0C region which is the DTCM (DMA can't access this region).
I have tried changing the "RAM" to "RAM_D2" that didn't do anything.
The only way I got it to change was change the DMA buffer to a static then change the linker, however I dont want it to be static.
I also notice when I change any of the linker .bss or .data anytime I try to insert a new() into an array it hardfaults now.
Linker file:
/*
******************************************************************************
**
** File : LinkerScript.ld
**
** Author : STM32CubeIDE
**
** Abstract : Linker script for STM32H7 series
** 2048Kbytes FLASH and 192Kbytes RAM
**
** Set heap size, stack size and stack location according
** to application requirements.
**
** Set memory bank area and size if external memory is used.
**
** Target : STMicroelectronics STM32
**
** Distribution: The file is distributed as is, without any warranty
** of any kind.
**
*****************************************************************************
** @attention
**
** Copyright (c) 2019 STMicroelectronics.
** All rights reserved.
**
** This software component is licensed by ST under BSD 3-Clause license,
** the "License"; You may not use this file except in compliance with the
** License. You may obtain a copy of the License at:
** opensource.org/licenses/BSD-3-Clause
**
****************************************************************************
*/
/* Entry Point */
ENTRY(Reset_Handler)
/* Highest address of the user mode stack */
_estack = 0x20020000; /* end of RAM */
/* Generate a link error if heap and stack don't fit into RAM */
_Min_Heap_Size = 0x200 ; /* required amount of heap */
_Min_Stack_Size = 0x400 ; /* required amount of stack */
/* Specify the memory areas */
MEMORY
{
FLASH (rx) : ORIGIN = 0x08000000, LENGTH = 2048K
RAM (xrw) : ORIGIN = 0x20000000, LENGTH = 128K
RAM_D1 (xrw) : ORIGIN = 0x24000000, LENGTH = 512K
RAM_D2 (xrw) : ORIGIN = 0x30000000, LENGTH = 288K
RAM_D3 (xrw) : ORIGIN = 0x38000000, LENGTH = 64K
ITCMRAM (xrw) : ORIGIN = 0x00000000, LENGTH = 64K
}
/* Define output sections */
SECTIONS
{
/* The startup code goes first into FLASH */
.isr_vector :
{
. = ALIGN(4);
KEEP(*(.isr_vector)) /* Startup code */
. = ALIGN(4);
} >FLASH
/* The program code and other data goes into FLASH */
.text :
{
. = ALIGN(4);
*(.text) /* .text sections (code) */
*(.text*) /* .text* sections (code) */
*(.glue_7) /* glue arm to thumb code */
*(.glue_7t) /* glue thumb to arm code */
*(.eh_frame)
KEEP (*(.init))
KEEP (*(.fini))
. = ALIGN(4);
_etext = .; /* define a global symbols at end of code */
} >FLASH
/* Constant data goes into FLASH */
.rodata :
{
. = ALIGN(4);
*(.rodata) /* .rodata sections (constants, strings, etc.) */
*(.rodata*) /* .rodata* sections (constants, strings, etc.) */
. = ALIGN(4);
} >FLASH
.ARM.extab : { *(.ARM.extab* .gnu.linkonce.armextab.*) } >FLASH
.ARM : {
__exidx_start = .;
*(.ARM.exidx*)
__exidx_end = .;
} >FLASH
.preinit_array :
{
PROVIDE_HIDDEN (__preinit_array_start = .);
KEEP (*(.preinit_array*))
PROVIDE_HIDDEN (__preinit_array_end = .);
} >FLASH
.init_array :
{
PROVIDE_HIDDEN (__init_array_start = .);
KEEP (*(SORT(.init_array.*)))
KEEP (*(.init_array*))
PROVIDE_HIDDEN (__init_array_end = .);
} >FLASH
.fini_array :
{
PROVIDE_HIDDEN (__fini_array_start = .);
KEEP (*(SORT(.fini_array.*)))
KEEP (*(.fini_array*))
PROVIDE_HIDDEN (__fini_array_end = .);
} >FLASH
/* used by the startup to initialize data */
_sidata = LOADADDR(.data);
/* Initialized data sections goes into RAM, load LMA copy after code */
.data :
{
. = ALIGN(4);
_sdata = .; /* create a global symbol at data start */
*(.data) /* .data sections */
*(.data*) /* .data* sections */
*(.RamFunc) /* .RamFunc sections */
*(.RamFunc*) /* .RamFunc* sections */
. = ALIGN(4);
_edata = .; /* define a global symbol at data end */
} >RAM AT> FLASH
/* Uninitialized data section */
. = ALIGN(4);
.bss :
{
/* This is used by the startup in order to initialize the .bss secion */
_sbss = .; /* define a global symbol at bss start */
__bss_start__ = _sbss;
*(.bss)
*(.bss*)
*(COMMON)
. = ALIGN(4);
_ebss = .; /* define a global symbol at bss end */
__bss_end__ = _ebss;
} >RAM
/* User_heap_stack section, used to check that there is enough RAM left */
._user_heap_stack :
{
. = ALIGN(8);
PROVIDE ( end = . );
PROVIDE ( _end = . );
. = . + _Min_Heap_Size;
. = . + _Min_Stack_Size;
. = ALIGN(8);
} >RAM
/* Remove information from the standard libraries */
/DISCARD/ :
{
libc.a ( * )
libm.a ( * )
libgcc.a ( * )
}
.ARM.attributes 0 : { *(.ARM.attributes) }
}
Where DMA buffer gets delcared
/*
* CLI.h
*
* Created on: Sep 22, 2021
* Author: Chris
*/
#ifndef TOOLS_CLI_CLI_H
#define TOOLS_CLI_CLI_H
#include <stdint.h>
#include "stm32h743xx.h"
#include "../../Constants/projectConfigure.h"
#include "../../Constants/functionReturnStates.h"
#include "../../Drivers/STM32H7xx_HAL_Driver/Inc/stm32h7xx_ll_usart.h"
#include "../../Drivers/STM32H7xx_HAL_Driver/Inc/stm32h7xx_ll_bus.h"
#include "../../Drivers/STM32H7xx_HAL_Driver/Inc/stm32h7xx_ll_dma.h"
#include "../../Drivers/STM32H7xx_HAL_Driver/Inc/stm32h7xx_ll_gpio.h"
#include "CMD/CMD.h"
class CLI {
private:
char CLI_TxBuff[CLI_buffLength] = {0};
char CLI_RxBuff[CLI_buffLength] = {0};
uint32_t baudRate;
void enableTx();
public:
CLI();
void execute(CMD * CMDs, char * CLI_TxBuff);
char * getCLITxBuff(void);
};
#endif /* TOOLS_CLI_CLI_H_ */
Solved! Go to Solution.
2021-09-28 06:36 PM
Replace all three instances of ">RAM" with ">RAM_D1" and change the _estack definition to "_estack = ORIGIN(RAM_D1) + LENGTH(RAM_D1);"
2021-09-28 06:36 PM
Replace all three instances of ">RAM" with ">RAM_D1" and change the _estack definition to "_estack = ORIGIN(RAM_D1) + LENGTH(RAM_D1);"
2021-09-28 06:40 PM
2021-09-28 06:40 PM
Well, that did it good sir, went from 0x2001 -> 0x2400
2021-09-28 06:44 PM
@TDK Only problem now is that the DMA isnt transferring anything from the buffer to the peripheral