STM32G474VET NOT CONNECT THE JTAG
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2024-07-24 1:29 AM
I my micro controller not debugging in JTAG MODE it is perfectly working in the working SWD mode.Whenever I tried to connect using JTAG it showing error (DEV_CONNECT_ERR) cause by the time of opening C:\ST\STM32CubeIDE_1.12.0\STM32CubeIDE\plugins\com.st.stm32cube.ide.mcu.externaltools.cubeprogrammer.win32_2.0.600.202301161003\tools\bin\STM32_Programmer_CLI.exe.Please try to help me
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2024-08-13 3:45 AM
Hello @KayalaSandeep and welcome to the community :),
Please use the "Scan" option to detect the ST-Link. When [ST-LINK S/N] is enabled, the serial number of the ST-LINK probe to be used must be entered in the edit/ list field. The [Scan] button can be used to scan and list all detected ST-LINK devices connected to the PC. please take a look at STM32CubeIDE user guide - User manual.
Also, make sure that your ST-Link firmware is up to date.
Could you please check your hardware may this application note can help you "Getting started with STM32G4 Series
hardware development boards"
Thank you.
Kaouthar
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.