cancel
Showing results for 
Search instead for 
Did you mean: 

STM32CubeIDE suddently stop to Debug and Run

SScar.2
Senior

Hi there, 

I'm facing a problem with Cube IDE (ver. 1.13.0). Completely out of nowhere, it stopped letting me debug or run the code. When I click the buttons, I can see in the bottom right corner that it tries to launch the debugger, but it stops at Launching XXXX Debug: 0% and immediately disappear. 

I already tried to reinstall everything, but nothing happened. I also tried to start the GDB server manually but nothing... 
Actually, the board and ST-Link (V3MINI) are OK, and I can program the board through STM32Programmer. 

Can anybody please help me? I can't work like that...

Thanks 

Simone

1 ACCEPTED SOLUTION

Accepted Solutions
Souhaib MAZHOUD
ST Employee

Hi @SScar.2 

Thank you for posting.

Have you tried the last version STM32CubeIDE 1.13.1, otherwise could you share the name of the board you using?

Thank you

Souhaib

View solution in original post

2 REPLIES 2
Souhaib MAZHOUD
ST Employee

Hi @SScar.2 

Thank you for posting.

Have you tried the last version STM32CubeIDE 1.13.1, otherwise could you share the name of the board you using?

Thank you

Souhaib

Actually I just SOLVED (after a lot of hours spent with this problem). I just erased the whole .metadata folder from workspace directory and it worked! Absolutely no idea why. 

Thanks however for the help