2023-11-28 9:36 PM
I have developing my project for some weeks now with no issues, then suddenly I cannot open the IOC file to modify the pin configuration. Worked on Monday, doesn't work two days later. no files have been copied or duplicated, just pushed to git.
I have tried all the updates I can find but still no joy.
The error message is:
Invalid Input: Must be project's active .ioc file.
Project's 'XXX-011-Firmware' active one is 'XX-011-Firmware.ioc' file
I am using Cube:
Version: 1.14.0
Build: 19471_20231121_1200 (UTC)
I have looked in the IOS file and:
ProjectManager.ProjectFileName=XXX-011-Firmware.ioc
ProjectManager.ProjectName=XXX-011-Firmware
Match
IDE Log Attached
Last successful .ide.log (MX) two days earlier attached.
No new logs created because of the error.
Can anyone help?
2023-11-28 11:58 PM
Welcome @Bob_Walton,to the community!
The error message appears, for example, if there is more than one IOC in the project or if the IOC file has been renamed (as in this case).
Regards
/Peter
2023-11-29 12:01 PM
The file has not been renamed and there is only one IOC file in the project.
I did manage to recover by doing the following.
BUT
if I edit the settings and code generation takes place, I cannot open the file again without repeating the steps above.
I would seem that code generation locks the file.
Regards
Bob
2023-11-29 12:14 PM
What if you run CubeMX stand-alone instead of starting it from inside the IDE?
<soapbox>I never run CubeMX from inside the IDE. I always run the stand-alone version. For me it is just plain easier, and quicker when I'm working for multiple projects at the same time.</soapbox>
2023-11-30 12:33 AM
@Bob_Walton With steps 1 to 3, you are obviously creating an (essentially) identical IOC to the previous IOC - except that the process blocking the previous one does not yet have access to it. Step 4 shows that the new IOC still contains a reference to an older firmware library, which is why you are offered the migration.
Generating code does not block the IOC, but I suspect some cloud functionality does. Didn't you mention that you are working with GIT?
2023-11-30 12:13 PM
@Peter BENSCH Yes, I am using GuiHub as the repository for pushing my code changes. Do you suspect there is a link between the push and the IOC read problem?
At the end of each day I push my repo, so the fact that the problem appears between two days seems to be a viable root cause.
Why would the IOC link be broken by a git push?
I Have been working with Git all along and this problem only started recently. Is there some background update which I am not aware of?
2023-12-01 12:27 AM
I cannot tell you the exact cause, but I have experienced something similar when a file that is currently being edited is to be deleted.
I suspect that the synchronization process is still active and is therefore blocking the IOC. You would have to check whether this is the case and how you can get this process to release the file again after synchronization.