2024-02-22 09:21 PM - edited 2024-02-22 09:51 PM
Hi,
I am using STM32CubeIDE to build project fro STM32H753 microcontroller.
I am unaware why the STM32CubeIDE is updating the type of uint32_t to unsigned long.
I assume for a 32 bit processor uint32_t should be typed to unsigned int.
Where do I find declaration of __UINT32_TYPE__ ?
/* Sample code to report issue */
uint32_t my_id = "1234";
sprintf( tmpstr, "Ser# %08X\r\n", my_id );
On compiling code I observe:
../User_Code/File_Xxx.c:205:36: warning: format '%X' expects argument of type 'unsigned int', but argument 3 has type 'uint32_t' {aka 'long unsigned int'} [-Wformat=]
205 | sprintf( tmpstr, "Ser# %08X\r\n", my_id );
| ~~~^ ~~~~~~~~~~~~
| | |
| | uint32_t {aka long unsigned int}
| unsigned int
| %08lX
Is there a way I can instruct STM32CubeIDE to type case uint32_t to unsigned int.
I also want to ensure that my change is not overwritten when I regenerate the code with help of IOC file.
Regards,
Rajeev
Solved! Go to Solution.
2024-02-23 03:56 AM
The correct way to do this is to use the format specifiers from inttypes.h; eg, PRIx32 for uint32_t
eg,
uint32_t my_id = "1234";
sprintf( tmpstr, "Ser# %08" PRIx32 "\r\n", my_id );
https://en.wikibooks.org/wiki/C_Programming/inttypes.h
BTW: Use this button to get the code formatting:
2024-02-23 03:56 AM
The correct way to do this is to use the format specifiers from inttypes.h; eg, PRIx32 for uint32_t
eg,
uint32_t my_id = "1234";
sprintf( tmpstr, "Ser# %08" PRIx32 "\r\n", my_id );
https://en.wikibooks.org/wiki/C_Programming/inttypes.h
BTW: Use this button to get the code formatting:
2024-02-23 04:23 AM - edited 2024-02-23 04:25 AM
Thanks! I will test it out.
2024-02-23 06:28 AM
> uint32_t my_id = "1234";
This won't even compile.
Unable to reproduce the issue even if I take out the quotes.
2024-02-23 07:23 AM - edited 2024-02-23 07:32 AM
@TDK wrote:This won't even compile.
It will compile, but with a warning about that initialiser:
warning: initialization of 'uint32_t' {aka 'long unsigned int'} from 'char *' makes integer from pointer without a cast [-Wint-conversion]
😎
EDIT
In addition to the OP's warning:
warning: format '%x' expects argument of type 'unsigned int', but argument 3 has type 'uint32_t' {aka 'long unsigned int'} [-Wformat=]
65 | sprintf( tmpstr, "Ser# %08x\r\n", my_id );
| ~~~^ ~~~~~
| | |
| | uint32_t {aka long unsigned int}
| unsigned int
| %08lx
2024-02-23 08:46 AM
Unfortunately even for 32-bit platform, GCC and the newlib library define int32_t as long. Even though int and long are same physical types, the compiler distinguishes them and requires printf format %ld or %lu. Or %lX.
Agree with Andrew about inttypes.h, but these format macros are maddening ((
2024-02-23 08:50 AM
@Pavel A. wrote:these format macros are maddening ((
Aren't they just?! 🙄😳
Could they have made it more klunky if they'd tried?
2024-02-23 09:01 AM
Well, the C++ way (ostream and operator << ) handles it automatically, but it takes conversion to C++. Variadic C functions are a headache.