2021-08-17 01:41 AM
Hi there,
I am having trouble with CubeIDE: When building my project i get the following error:
"fatal error: core_cm4.h: No such file or directory"
I am using:
What I did to get to this point:
Hope someone can help me on this
Greetings MM1
Solved! Go to Solution.
2021-08-17 06:25 AM
Hello @MM1 ,
It seems the include paths are not properly set up.
Please make sure to configure the include paths and check the path of the core_cm4.h header file. Maybe that folder was not in the include folder list.
When your question is answered, please close this topic by choosing Select as Best. This will help other users find that answer faster.
Imen
2021-08-17 06:25 AM
Hello @MM1 ,
It seems the include paths are not properly set up.
Please make sure to configure the include paths and check the path of the core_cm4.h header file. Maybe that folder was not in the include folder list.
When your question is answered, please close this topic by choosing Select as Best. This will help other users find that answer faster.
Imen
2021-08-18 12:39 AM
Hi Imen,
Thanks for the reply. I double checked the include paths and the path to the core_cm4.h was indeed missing.
It is just sad that you have to do it manually sometimes when using the Toolchain MotorControl Workbench/CubeMX (happened to me before)
greeting MM1
2023-01-12 07:12 PM
hi, I know it has been a year ago, but may I know how to include the path? i mean how to find the path library and put it in the path?
2023-01-14 06:48 PM
Are you unable of finding files on your PC and using the internet?