cancel
Showing results for 
Search instead for 
Did you mean: 

STM32CubeIDE 1.17.0 released

Semer CHERNI
ST Employee

We are pleased to announce to you that the release 1.17.0 of STM32CubeIDE is available.

What is new in 1.17.0:

  • Microcontrollers, microprocessors, and board lists aligned with STM32CubeMX:
    • Added the support for the STM32N6 series
    • Added the support for the STM32U3 series.
    • Added the support for the STM32WL3x line
    • Added the support for the STM32MP23xx microprocessors
    • Added the support for the STM32MP25xx microprocessors in a TFBGA361 16 mm × 16 mm package
    • Added the support for new microcontrollers in the STM32C0 series and related Nucleo boards (NUCLEO-C051C8 and NUCLEO-C092RC)
    • Added the support for new microcontrollers in the STM32G4 series
    • Added the support for new microcontrollers in the STM32WBA series and the related B-WBA5M-WPAN board
  • Simplified user authentication interface
  • Added support for debug authentication with password for the STM32N6 series.
  • Improved support of OpenSTLinux plugin to be version agnostic
  • Enabled the installation of both STM32MP1 and STM32MP2 flavors of OpenSTLinux plugins within the same STM32CubeIDE instance.
  • Added support for flashing the .bin file during debugging.

Main fixed issues in 1.17.0:

Refer to the STM32 microcontroller wiki at:
wiki.st.com/stm32mcu/wiki/Category:STM32CubeIDE_errata

Known problems and limitations in 1.17.0:

Refer to the STM32 microcontroller wiki at:
wiki.st.com/stm32mcu/wiki/Category:STM32CubeIDE_errata

How to get STM32CubeIDE 1.17.0:

  • Under this link
  • Or update your current installation of STM32CubeIDE using: Help > Check for updates (The in-tool update does not allow updating the drivers and ST-LINK server tool. Full installation is required for this to be done).

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

12 REPLIES 12
padawan
Senior

Hi STM,

you fixed this asap .....not.

https://community.st.com/t5/stm32cubeide-mcus/stm32cubeide-1-14-0-gt-old-issue/m-p/612850

or 

https://community.st.com/t5/stm32cubeide-mcus/jumping-to-random-file-after-pressing-run-button/td-p/246693/page/12

 

This is a longstanding bug (over 4 years). and again:

Opening an internal ticket is not a solution, it is poor.

padawan


@Semer CHERNI wrote:

Known problems and limitations in 1.17.0:

Refer to the STM32 microcontroller wiki at:
wiki.st.com/stm32mcu/wiki/Category:STM32CubeIDE_errata.


That link doesn't work:

AndrewNeil_0-1732788774544.png

There's a spurious full stop on the end.

The previous link to the same page is OK.


@padawan wrote:

Opening an internal ticket is not a solution


It isn't even mentioned in the 'Known Issues'.

Hello @padawan 

First let me thank you for posting.

It's well understood that this behavior create frustration to users.

The issue is under analysis from our team. The issue is linked to Eclipse version used by STM32CCubeIDE and it should be fixed when the Eclipse is updated.

Our teams are doing there best to fix this and any other defect to provide the best user experience.

KR,
Semer.

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.


@Semer CHERNI wrote:

It's well understood that this behavior create frustration to users.


So why is it not even listed in the 'Known Issues', then?

hi Andrew,

 

The extra character in the url was suppressed.

Thank you for telling us

 

Hello Andrew,

 

You're right, it's an oversight. I've added it in the list.

My apologies

 

For the issue itself, we are dependent on Eclipse integration.

Thank you

Christelle 

Hello Cristelle

162500After programming a device in Run mode, STM32CubeIDE opens every time a new tab with startup file and give focus on that tab.

it open not only the startupfile "*.s". It open randomly files. like .c or .cpp.

If you have a new project and debug it at the first time, it is not showning this behavior.

If you debug the project after this, a second or more one, it opens randomly files form the project.

padawan 

What us the release planning? Once we upgrade to this version how long we can expect support on this version? Or when we file bug, will you say, if you want, upgrade and try yourself?

If you feel a post has answered your question, please click "Accept as Solution".