2024-11-27 12:42 AM - edited 2024-12-11 8:44 AM
We are pleased to announce to you that the release 1.17.0 of STM32CubeIDE is available.
Refer to the STM32 microcontroller wiki at:
wiki.st.com/stm32mcu/wiki/Category:STM32CubeIDE_errata
Refer to the STM32 microcontroller wiki at:
wiki.st.com/stm32mcu/wiki/Category:STM32CubeIDE_errata
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2024-11-28 12:42 AM
Hi STM,
you fixed this asap .....not.
https://community.st.com/t5/stm32cubeide-mcus/stm32cubeide-1-14-0-gt-old-issue/m-p/612850
or
This is a longstanding bug (over 4 years). and again:
Opening an internal ticket is not a solution, it is poor.
padawan
2024-11-28 2:14 AM
@Semer CHERNI wrote:Known problems and limitations in 1.17.0:
Refer to the STM32 microcontroller wiki at:
wiki.st.com/stm32mcu/wiki/Category:STM32CubeIDE_errata.
That link doesn't work:
There's a spurious full stop on the end.
The previous link to the same page is OK.
2024-11-28 2:17 AM
@padawan wrote:Opening an internal ticket is not a solution
It isn't even mentioned in the 'Known Issues'.
2024-11-28 2:36 AM
Hello @padawan
First let me thank you for posting.
It's well understood that this behavior create frustration to users.
The issue is under analysis from our team. The issue is linked to Eclipse version used by STM32CCubeIDE and it should be fixed when the Eclipse is updated.
Our teams are doing there best to fix this and any other defect to provide the best user experience.
KR,
Semer.
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2024-11-28 2:48 AM
@Semer CHERNI wrote:It's well understood that this behavior create frustration to users.
So why is it not even listed in the 'Known Issues', then?
2024-11-28 6:59 AM - edited 2024-11-28 7:46 AM
hi Andrew,
The extra character in the url was suppressed.
Thank you for telling us
2024-11-28 7:06 AM - edited 2024-11-28 7:45 AM
Hello Andrew,
You're right, it's an oversight. I've added it in the list.
My apologies
For the issue itself, we are dependent on Eclipse integration.
Thank you
Christelle
2024-11-28 10:59 PM
Hello Cristelle
162500 | After programming a device in Run mode, STM32CubeIDE opens every time a new tab with startup file and give focus on that tab. |
it open not only the startupfile "*.s". It open randomly files. like .c or .cpp.
If you have a new project and debug it at the first time, it is not showning this behavior.
If you debug the project after this, a second or more one, it opens randomly files form the project.
padawan
2024-11-30 6:59 PM
What us the release planning? Once we upgrade to this version how long we can expect support on this version? Or when we file bug, will you say, if you want, upgrade and try yourself?