Skip to main content
Semer CHERNI
ST Employee
November 27, 2024
Question

STM32CubeIDE 1.17.0 released

  • November 27, 2024
  • 14 replies
  • 6900 views

We are pleased to announce to you that the release 1.17.0 of STM32CubeIDE is available.

What is new in 1.17.0:

  • Microcontrollers, microprocessors, and board lists aligned with STM32CubeMX:
    • Added the support for the STM32N6 series
    • Added the support for the STM32U3 series.
    • Added the support for the STM32WL3x line
    • Added the support for the STM32MP23xx microprocessors
    • Added the support for the STM32MP25xx microprocessors in a TFBGA361 16 mm × 16 mm package
    • Added the support for new microcontrollers in the STM32C0 series and related Nucleo boards (NUCLEO-C051C8 and NUCLEO-C092RC)
    • Added the support for new microcontrollers in the STM32G4 series
    • Added the support for new microcontrollers in the STM32WBA series and the related B-WBA5M-WPAN board
  • Simplified user authentication interface
  • Added support for debug authentication with password for the STM32N6 series.
  • Improved support of OpenSTLinux plugin to be version agnostic
  • Enabled the installation of both STM32MP1 and STM32MP2 flavors of OpenSTLinux plugins within the same STM32CubeIDE instance.
  • Added support for flashing the .bin file during debugging.

Main fixed issues in 1.17.0:

Refer to the STM32 microcontroller wiki at:
wiki.st.com/stm32mcu/wiki/Category:STM32CubeIDE_errata

Known problems and limitations in 1.17.0:

Refer to the STM32 microcontroller wiki at:
wiki.st.com/stm32mcu/wiki/Category:STM32CubeIDE_errata

How to get STM32CubeIDE 1.17.0:

  • Under this link
  • Or update your current installation of STM32CubeIDE using: Help > Check for updates (The in-tool update does not allow updating the drivers and ST-LINK server tool. Full installation is required for this to be done).
This topic has been closed for replies.

14 replies

padawan
Senior
November 28, 2024

Hi STM,

you fixed this asap .....not.

https://community.st.com/t5/stm32cubeide-mcus/stm32cubeide-1-14-0-gt-old-issue/m-p/612850

or 

https://community.st.com/t5/stm32cubeide-mcus/jumping-to-random-file-after-pressing-run-button/td-p/246693/page/12

 

This is a longstanding bug (over 4 years). and again:

Opening an internal ticket is not a solution, it is poor.

padawan

Andrew Neil
Super User
November 28, 2024

@padawan wrote:

Opening an internal ticket is not a solution


It isn't even mentioned in the 'Known Issues'.

A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.
Andrew Neil
Super User
November 28, 2024

@Semer CHERNI wrote:

Known problems and limitations in 1.17.0:

Refer to the STM32 microcontroller wiki at:
wiki.st.com/stm32mcu/wiki/Category:STM32CubeIDE_errata.


That link doesn't work:

AndrewNeil_0-1732788774544.png

There's a spurious full stop on the end.

The previous link to the same page is OK.

A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.
christelle burguera
ST Employee
November 28, 2024

hi Andrew,

 

The extra character in the url was suppressed.

Thank you for telling us

 

Explorer
December 3, 2024

myST -> Login does not work properly on Linux Mint (ubuntu 22 based). I needed to work on some stm32 code pronto today, have a new machine so naturally I downloaded the latest and installed it. Big mistake. It forced me to login repeatedly then promptly forgot, went to myST -> Login and entered my account, then tried to download packages from Help | Manage Embedded Software without luck. cube finder was unable to download the packages too. Finally, I uninstalled 1.17 then reinstalled 1.12. Fortunately, I had a copy of the installer, since it is gone from st.com

Please get rid of this login ***. I have wasted hours. I will not recommend stm32 for future projects if this *** continues. It's prob too late to change for this project, but fortunately 1.12 still works OK

Explorer
February 5, 2025

STM32WB07CC Programming Error on Linux due to Case Sensitivity in Memory Definition File Name

Dear STMicroelectronics,

I am writing to report an error I encountered while trying to program an STM32WB07xx microcontroller using STM32CubeIDE 1.17.0 on a 64-bit Linux system.

Problem:

When attempting to program the device, the following error message is displayed in the log:

Warning: No flash region defined for device id 0x1e

Steps to Reproduce:

  1. Create a new project for STM32WB07xx in STM32CubeIDE.
  2. Configure the project and generate the code.
  3. Attempt to program the microcontroller.

Cause:

The issue is related to the case sensitivity of the Linux file system. STM32CubeIDE (or a tool it uses) is looking for the memory definition file named "0x1e.stldr", but the actual file on the file system is named "0x1E.stldr".

Solution:

Renaming the file "0x1E.stldr" to "0x1e.stldr" resolves the problem.

Suggested Improvement:

I suggest that STMicroelectronics implement a solution in STM32CubeIDE to handle this case sensitivity difference on Linux systems. For example, the IDE could ignore capitalization when searching for files, or offer a configuration option to disable case sensitivity.

Thank you for your attention to this matter. I hope this report is helpful for improving STM32CubeIDE.

Sincerely,