2024-08-03 11:23 AM
Hello,
I updated to Mac15 (MacOS Sonoma Public Beta), which was probably a mistake. Now I get an error from STMCubeIDE when I try to run indicating "ST-Link Server is required to launch the debug session" and to Please download it on www.st.com.
I figured something changed in the OS that no longer makes the ST-Link Server run any more.
However when I try to download it, I get essentially a broken link, or at least it simply wont download. Even worse, the web page with Safari seems entirely broken and I cant even get a download to start after accepting the license, but with FireFox I get further, I get but still wont download and the link seems broke.
I can still flash using the STM32CubeProgrammer fortunately (using 2.13.1).
Can anyone tell me how to download this ST-Link Server? Or if there is an issue with the last MacOS and this and there is no fix?
Solved! Go to Solution.
2024-09-15 10:04 AM
Rohdea, I made an ST account specifically to thank you. You saved me such a hassle. Thanks!!!
2024-09-20 10:03 AM
Gracias por la solución, funciona bien con con la versión 15.0 oficial, espero que solucionen pronto el problema de incopatibilidad. Nuevamente GRACIAS!!!!!!!
2024-09-21 07:22 AM
That works for me! Thanks!
2024-09-21 09:04 AM
macOS 15 not yet supported.
possible solution :
run the following command in the external terminal, the GDB server starts properly, and I'm able to debug the application. I use then remote GDB server (localhost with default port)
This starts the GDB server and loads my application without any issues.
2024-09-24 11:42 PM
Thanks, It worked!