cancel
Showing results for 
Search instead for 
Did you mean: 

Sources missing from CubeIDE project...

NicRoberts
Associate II

Hi, 

STMCubeIDE 1.17.0

I opened & built an example project for the NULCEO WB55. It built successfully & download onto the board & runs as expected. But when I tried to add some functionality to the code by clicking on the file in the project navigator all the files are missing!

missing_sources.png

4 REPLIES 4

Are they there is you look in the Windows Explorer?

No it looks different in Explorer

cube_odd.png


@NicRoberts wrote:

it looks different in Explorer


Indeed - the "folders" within the Project aren't (necessarily) folders in the underlying host file system.

But can you find the files at all ?

Found them under `Application : User : Core` in the project manager. I take it this will always be the case when exporting from MX?