cancel
Showing results for 
Search instead for 
Did you mean: 

Source File

DYann.1
Senior II

Hello,

After after installing version Version: 1.13.1 (I have before the 1.8.0). I can open my Projet and compile with no errors. But when I'm in Debug mode I can't see my code but I have this message : 

DYann1_0-1697647776539.png

What does that mean ? The source file I can see :

DYann1_1-1697647975585.png

Do you know how to proceed ?

Thank you for your helps.

Regards

17 REPLIES 17
Bob S
Principal

The error mentions path with "workspace_1.8.0" in the path, whereas your IDE image says "workspace_1.13.1" in the path.  Where are the files REALLY located? 

The file is located in the in the workspace_1.13.1 : 

DYann1_0-1697698164299.png

I think for the first time I created this project under version 1.18.0 and when I make a copy to put in the 1.13.1 directory it still sees the dependency initially created. So how to how to open under workspace_1.13.1 ?

padawan
Senior

Hi,

can you import the old (1.8) project?

padawan_0-1697714554436.png

padawan_1-1697714695715.png

An if it not work:

look at the ".launch" file with the editor and replace all "1.8.0" with "1.13.1"

HTH

Padawan

Hi,

What do you mean import the old projet ? I suppose under STMCubeIDE (1.13.1) I import the old projet probably ? I encounter this screen

DYann1_0-1697718045007.png

So what should I select please ? Thank you for your answer. I can guess your message at the bottom right of the screen I can select this directory

DYann1_0-1697718427207.png

And I can see the projet like this picture :

DYann1_1-1697718470615.png

I can compile without errors but always the same screen when I'm in DEBUG mode :

DYann1_2-1697718713022.png

I also modified the .launch file to 1.13.1 but I still have the same error. 

DYann1_3-1697719118885.png

 

 

 

Take a look at 

padawan_0-1697721352753.png

Use the "searchProject" or better "Browse" to your

padawan_1-1697721403090.png

 

 "debug" and there select the .elf file.

it seems that there is an old path in the config....

hth

Padawan

 

to get the right elf file.

 

 

padawan
Senior

What happen if you click on "locate the file"? Can you see your .s File?

hth

Padawan 

 

Hi,

Always the same error :

DYann1_0-1697722205008.png

DYann1_1-1697722249025.png

I can see always the path workspace_1.8.0/SGTL_5000_v00/Debug.....

When I click on locate the file :

DYann1_0-1697722777171.png

I can see this picture :

DYann1_1-1697722841615.png

And bottom right I have this message : 

DYann1_2-1697722947685.png

And effectively in this directory :

DYann1_3-1697723016112.png

I have nothing. 

I think you have to search your .s file in the startupfolder bleow debug.

if there more than 1 .s file delete them.

Another tip

padawan_0-1697723082249.png

May be it helps.

May be a reboot can help.

May be save your work (zip) cleanup (delete the workspace) unpack you work in a dir on the dDesktop and import his dir  by "Open Projects from File system".

it gets darker, The last stm32cubeIDE is 1.13.2...

 

padawan