cancel
Showing results for 
Search instead for 
Did you mean: 

Yellow flagged pin conflict information pops up too short to read (macOS)

chriskuku
Senior III

When being in the MX (.ioc) file view hovering over a yellow marked TIM1 e.g., a grey field pops up for half of a second. I'm hardly able to read and understand the sense, too short is the presence of that field. Can it be looked up elsewhere in the GUI. It says something of "partly disabled,a conflict with PB13 being used as an output" or so.

 

3 REPLIES 3
TDK
Super User

PB13 can be TIM1_CH1N. If you're using the pin as GPIO, this channel of the timer can't be enabled.

The yellow flags do not indicate errors, just that you can't do something because a pin is being used. They can be safely ignored as they do not indicate an error.

If you feel a post has answered your question, please click "Accept as Solution".

Thanks. My question was: why does the tooltip flash up too shortly to read it. Is it a macOS problem/issue?

 

Yes, it seems to be a MacOS-specific issue.

If you feel a post has answered your question, please click "Accept as Solution".