cancel
Showing results for 
Search instead for 
Did you mean: 

Cubemx is not updating the links .project file in cubeIDE

gmn
Associate II

Very late response, but I was having the same issue with cubemx v6.14.0 working with stm32h755zit3u on a nucleo-h755zi dev-board and using stm32cubeIDE v1.8.0.  After some investigation, cubemx is not updating the links .project file in cubeIDE.  The .project file is just xml, so manually edit it and add links to stm32h7xx_hal_adc.c and stm32h7xx_hal_adc_ex.c (substitute h7xx for correct uC version for your project).

Possibly, I have set up something incorrectly in cubeMX - I'm just learning ADCs.  But, re-hitting the "generating code" button in cubeMX did not wipe out the my .project edits.  So, at least a temporary fix.

 

1 REPLY 1
TDK
Super User

Please include the IOC file you are having issues with so the issue can be replicated.

If you feel a post has answered your question, please click "Accept as Solution".