2024-04-23 11:56 AM
Hello,
I have an issue when I tried enter myST on STM32CubeIDE 1.15.0 version. Program shows second image and close itself how can I solve this issue?
Best regards.
2024-04-24 02:58 PM
Hello @BArsl.1,
Try to put the CubeMX firmware update in offline mode. (Preferences > STM32Cube > Firmware Updater)
Then, restart STM32CubeIDE.
Otherwise, please share the crash Report or log from the Console application, for more analysis.
2024-09-25 03:05 PM - edited 2024-09-25 03:21 PM
Hi,
I have the same issue and putting firmware update in offline mode doesn't seem to work. How can I get logs from STM32CubeIDE?
Best regards
EDIT: I managed to locate the logs file, could you look into it?
EDIT2: Of course after posting a reply, CubeMX suddenly updated itself and CubeIDE works fine... I will leave this reply for people with the same problem, maybe with logs you could find where the problem was.
2024-09-26 02:40 AM - edited 2024-09-26 02:41 AM
Hi @wiewiór and welcome to the ST Community
I share this article that may help Community users to set the network connection for STM32CubeMX and STM32CubeIDE :
How to set the network connection parameters for S... - STMicroelectronics Community
2024-11-04 07:17 AM
I have the exact same Problem, but Cubeide closes so fast, that i cant open the preferences to change the Firmware upgrader.
Reinstallation also did not work.
WIth old and the newest Software.
Also the Error Message Window is so fast that i only was able to see the Error with screen recording.