cancel
Showing results for 
Search instead for 
Did you mean: 

SelfUpgrade Update. Trying to restore.

BArsl.1
Associate II

Hello,

I have an issue when I tried enter myST on STM32CubeIDE 1.15.0 version. Program shows second image and close itself how can I solve this issue? 

login.pngSelfUpgrade Updaate.png

Best regards.

4 REPLIES 4
Imen.D
ST Employee

Hello @BArsl.1,

Try to put the CubeMX firmware update in offline mode. (Preferences > STM32Cube > Firmware Updater)

Then, restart STM32CubeIDE.

Otherwise, please share the crash Report or log from the Console application, for more analysis.

When your question is answered, please close this topic by clicking "Accept as Solution".
Thanks
Imen

Hi, 
I have the same issue and putting firmware update in offline mode doesn't seem to work. How can I get logs from STM32CubeIDE? 
Best regards

EDIT: I managed to locate the logs file, could you look into it? 
EDIT2: Of course after posting a reply, CubeMX suddenly updated itself and CubeIDE works fine... I will leave this reply for people with the same problem, maybe with logs you could find where the problem was. 

Hi @wiewiór and welcome to the ST Community 

I share this article that may help Community users to set the network connection for STM32CubeMX and STM32CubeIDE :

How to set the network connection parameters for S... - STMicroelectronics Community

When your question is answered, please close this topic by clicking "Accept as Solution".
Thanks
Imen
CJ_98
Associate

I have the exact same Problem, but Cubeide closes so fast, that i cant open the preferences to change the Firmware upgrader.
Reinstallation also did not work.
WIth old and the newest Software.

Also the Error Message Window is so fast that i only was able to see the Error with screen recording.