2025-02-14 03:25 AM
Win 10, x64, STM32CubeIDE version 1.17.0
I'm trying to open a CubeIDE project from a workspace but it just doesn't load, see image below.
I select the folder for my workspace, click finish & am then told that there are no projects in the folder. Yet the folder does contain a CubeIDE project. The open project option is also greyed out in the projects menu pull down.
What am I missing here?
2025-02-14 04:39 AM
Please see this thread which probably answers your question.
Regards
/Peter
2025-02-14 05:19 AM - edited 2025-02-14 05:56 AM
Turns out I was not in the workspace directory from where the project was created, which was further up the directory hierachy.
2025-02-14 07:09 AM
Hello @NicRoberts ,
If you solved your issue please accept your comment as solution.
Thank you.
2025-02-14 07:23 AM
I have identical problem with the version 1.17, I also have a lot of problems with version 1.17, I also ghastly sad because of problems of CubeIDE :( really sad.