2024-03-21 7:11 AM - edited 2024-03-21 7:14 AM
Hello.
After updating STM32CubeIDE to 1.15.0 I faced this problem :(
I can't run or debug any projects. Of course, software for STLink was updated.
Hope, someone has a solution.
My console includes this information:
Encountered Error when opening ..........\com.st.stm32cube.ide.mcu.externaltools.cubeprogrammer.win32_2.1.200.202311302303\tools\bin\STM32_Programmer_CLI.exe
Main alert
Error in final launch sequence:
Failed to execute MI command:
load ...........\\G030F6_test2\\Debug\\G030F6_test2.elf
Error message from debugger back end:
Error finishing flash operation
Failed to execute MI command:
load ...........\\G030F6_test2\\Debug\\G030F6_test2.elf
Error message from debugger back end:
Error finishing flash operation
Failed to execute MI command:
load ...........\\G030F6_test2\\Debug\\G030F6_test2.elf
Error message from debugger back end:
Error finishing flash operation
Error finishing flash operation
Solved! Go to Solution.
2024-04-04 3:59 AM
Thank you. I had reinstaled my OS and new CubeIDE started to work.
2024-03-21 7:39 AM - edited 2024-03-21 7:40 AM
Hello @DmitriG and welcome to the Community,
This issue is reported internally for more investigation via Internal ticket number: 176694.
(PS: Internal ticket number is only for reference, not available outside of ST)
2024-03-27 6:30 AM
Hello @DmitriG ,
According to the attachment it seems that you are using an older Windows version, but CubeIDE is only supported for Windows 10 and 11. This might affect the IDE functionality.
Regards,
Rim.
2024-04-01 4:34 PM
Hello Rim,
I get the exact same message. When you get an aswer please send it me.
I am running the laterst version of Windows 10, and IDE.
This problem also shows up when trying to do an upload on STM32CubePGR.
Jerry at jerry@game-finder.com
Thanks
2024-04-04 3:59 AM
Thank you. I had reinstaled my OS and new CubeIDE started to work.