cancel
Showing results for 
Search instead for 
Did you mean: 

Old AC6 Project fails on TruStudio and STM32CubeIDE

New.Fish
Associate III

We have a more than 10 years old STM32F100 project which was built by AC6, I try to use TruStudio and STM32CubeIDE 1.6.1 to import , and build it, but all fails on Error "Program "make" not found in path".

 

How to fix it?

1 ACCEPTED SOLUTION

Accepted Solutions

Did you follow the steps described in the UM2609 / 2.1.3 Importing existing projects

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.

View solution in original post

4 REPLIES 4

@New.Fish wrote:

STM32CubeIDE 1.6.1 


Is that a typo? The current version is 1.16.0

If you just use STM32CubeIDE to create a brand new project from scratch - does that work?

SofLit
ST Employee

Hello,

Did you try the steps described in the UM2609 importing projects, especially the section 2.1.3 Importing existing projects:

SofLit_0-1726483672748.png

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.

Hi SofLit,

It prompt some warning message during converting, refer to attached image file.

Finally, the compiler pass to  build it now,  but it generate a log message, refer to the text file,

will this affect the debugging?

 

 

Did you follow the steps described in the UM2609 / 2.1.3 Importing existing projects

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.