cancel
Showing results for 
Search instead for 
Did you mean: 

Null Pointer exception when managing Debug config.. for TouchGFX prj

andrea venturi
Associate III

hello, i've got an issue when dealing with the Debug Config launcher.

the context is a Src tree coming from TouchGFX 4.10.0, the ST32F429-discovery sample prj, and then heavily derived for the businessl logic, but, of course didn't tweaked on the Makefile.

I used to build and test on Linux pretty smoothly, but the boss recently told me to make it working inside CubeIDE on Windows (he's sort of a point & click guy.. :) )

i made my way to import the source tree into a CubeIde (1.4.2) prj and fix the makefile up to be able to build the .elf/.hex/.bin artifacts, using the "Cross GCC" and "Gnu Make Builder". that's good!

Now i'm trying to setup a Debug config launcher to be able to flash the board through ST-Link V2 and debug with gdb but the editing of the Debug cfg is raising a java.lang.NullPointerException with not much more detail.. see below the relevant screenshot.

weird error.. does anybody have a clue what to look at?

what's that log file referenced in the err msg, any insight/tip?

bests

Andrea

0 REPLIES 0