2024-11-08 9:58 PM - last edited on 2024-11-11 4:19 AM by Andrew Neil
I have installed STM32Cubide v 1.16.1 on both linux as well as on windows machine. After installation i tried to create project creation. I select board which is (Nucleo F439ZI) then clicking on next finish --> it ask my for myST login --> Code generation pop up window came up and in tips asked me to do Project --> genrate code (Necessary firmware packages is misssing) once i click on ok project created with only .ioc file. Other file is missing.
--> from help i tried Check for target selector then manage embedded software packages --> my STlogin again came up and Connection time out message even if my internet is working fine.
--> is there any proxy related issse?
--> uplaoding snapshot of mine network connection setting.
--> also tired offline downloaded packages and upload form local still getting errror. (missing dependecy of packges)
--> I tried with so many settings kindly help me to solve this issue.offiline installation from local drive
network connection setting
myST login error
2024-11-11 4:14 AM
Hi @bhaveshk ,
Could you please double check that the required steps as described in How to set the network connection parameters for STM32CubeIDE and STM32CubeMX are followed properly?
-Amel
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.