cancel
Showing results for 
Search instead for 
Did you mean: 

NO STM 32 Target Found, Target No Device Found (Nucleo-F446RE)

cherrytasty
Associate

cherrytasty_0-1724635922479.png

cherrytasty_1-1724635956025.png

what should i do..?

 

1 ACCEPTED SOLUTION

Accepted Solutions
TDK
Guru

> Target voltage: 0.31 V

This is a power issue. No change of a chip working without a proper power supply. Ensure the power jumper is set correctly. Perhaps a part on the board got damage in the course of debugging. It sees the ST-Link chip, so the board is probably okay. Consider looking at the schematic to track down the power issue.

If you feel a post has answered your question, please click "Accept as Solution".

View solution in original post

4 REPLIES 4
mƎALLEm
ST Employee

Hello,

First check if you are using a data cable not a charging cable

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.
PS:
1 - This is NOT an online support (https://ols.st.com) but a collaborative space.
2 - Please be polite in your reply. Otherwise, it will be reported as inappropriate and you will be permanently blacklisted from my help.

Do you have code that's reconfiguring the PA13 / PA14 debug pins, or putting them in a low power or sleep state?

Do you observe this problem if you pull/set BOOT0 pin HIGH? Here your code on the device won't be running and potentially breaking things.

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
TDK
Guru

> Target voltage: 0.31 V

This is a power issue. No change of a chip working without a proper power supply. Ensure the power jumper is set correctly. Perhaps a part on the board got damage in the course of debugging. It sees the ST-Link chip, so the board is probably okay. Consider looking at the schematic to track down the power issue.

If you feel a post has answered your question, please click "Accept as Solution".