cancel
Showing results for 
Search instead for 
Did you mean: 

NO STM 32 Target Found, Target No Device Found (Nucleo-F446RE)

cherrytasty
Associate

cherrytasty_0-1724635922479.png

cherrytasty_1-1724635956025.png

what should i do..?

 

1 ACCEPTED SOLUTION

Accepted Solutions
TDK
Guru

> Target voltage: 0.31 V

This is a power issue. No change of a chip working without a proper power supply. Ensure the power jumper is set correctly. Perhaps a part on the board got damage in the course of debugging. It sees the ST-Link chip, so the board is probably okay. Consider looking at the schematic to track down the power issue.

If you feel a post has answered your question, please click "Accept as Solution".

View solution in original post

4 REPLIES 4
mÆŽALLEm
ST Employee

Hello,

First check if you are using a data cable not a charging cable

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.

Do you have code that's reconfiguring the PA13 / PA14 debug pins, or putting them in a low power or sleep state?

Do you observe this problem if you pull/set BOOT0 pin HIGH? Here your code on the device won't be running and potentially breaking things.

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
TDK
Guru

> Target voltage: 0.31 V

This is a power issue. No change of a chip working without a proper power supply. Ensure the power jumper is set correctly. Perhaps a part on the board got damage in the course of debugging. It sees the ST-Link chip, so the board is probably okay. Consider looking at the schematic to track down the power issue.

If you feel a post has answered your question, please click "Accept as Solution".