cancel
Showing results for 
Search instead for 
Did you mean: 

LL library STM32 OUTPUT compare preload pwm setting enable is unsuccessful,May I ask what is the reason?

Bence
Associate II

When I set Output compare preload to enable in the configuration interface, the generated code shows disable0693W000001cFw5QAE.png0693W000001cFvvQAE.png

This discussion is locked. Please start a new topic to ask your question.
13 REPLIES 13
waclawek.jan
Super User

Look 2 lines higher than is the highlight - there's the preload enable.

JW

Thank you for your answer. When I set Out put compare preload to disable in Device Configuration Tool, the highlight is still enable. I do n’t know how to configure to change these parameters. Could you tell me if you know?

0693W000001cIodQAE.png0693W000001cIoiQAE.png

My IDE version is 1.3.0

waclawek.jan
Super User

I don't know.

@Nesrine.JLASSI​ , can you please have a look at this?

Thanks,

JW

Hello @Bence​ 

Could you please share your ioc file to check the issue.

Best regards,

Nesrine

Hi, Nesrine . If you need any documents, please tell me。

Thank you all the same, JW

Hello @Bence​ 

The LL are a translation of the intropack HAL drive. So, if in the function of the driver that you call there is a forcing of this parameter, then it appears in the LL code generation. 

In the reference function you would call (if you are in HAL):

HAL_StatusTypeDef HAL_TIM_PWM_ConfigChannel(TIM_HandleTypeDef *htim,

                      TIM_OC_InitTypeDef *sConfig,

                      uint32_t Channel)

There's a call for channel preload.

0693W000001cM1LQAU.png

This is the code you find in LL.

Best regards,

Nesrine

waclawek.jan
Super User

Hi @Nesrine.JLASSI​

Why is then an option in the GUI to enable the preload, if it is ignored?

JW