cancel
Showing results for 
Search instead for 
Did you mean: 

STM32CubeIDE Changing the MCU/MPU project settings

danielbath
Associate

Hi, 

Usually I code in a terminal text editor, compile and flash my code in the command line. 

I used CubeMX to create a makefile, then modified the makefile to include certain commands I can run from the command line. I used OpenOCD and GDB to debug code from the command line. 
It is becoming a mission to do intense debugging where I can see the values of registers all at the same time. 
I would like the option to if required switch to STM32CubeIDE only for intense Debugging and do my normal coding with my current setup. 

I'm on Linux, I imported a Makefile project without being presented with the option of choosing the part. 
Now My project doesn't know which target I am compiling for. Is there any way to change these settings in CubeIDE ? It seems grayed out for me... Here is the error I'm getting 

Screenshot from 2026-05-25 19-58-04.png

 

Thanks, 

DJ

0 REPLIES 0