STM32CubeIDE (MCUs)

Ask questions on STM32CubeIDE. Discuss how to build, debug, configure, and optimize your project as well as how to use our software tools.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeIDE 2.1.1 released

We are pleased to announce that the minor version 2.1.1 of STM32CubeIDE is available. What is new in 2.1.1: This release covers the topics listed below: SEGGER J-Link GDB server updated to 9.24 to fix an issue with the Live Expression view during the...

Aimen1 by ST Employee
  • 1436 Views
  • 0 replies
  • 1 kudos

STM32CubeCLT 1.21.0 released

We are pleased to announce that STM32CubeCLT 1.21.0 release is available. What is new in 1.21.0: Maintenance of the previous version: Updated in accordance with STM32CubeIDE v2.1.0Update of Clang/LLVM toolchainUpdate of GCC to GCC 14Update of STM32Cu...

Aimen1 by ST Employee
  • 560 Views
  • 0 replies
  • 0 kudos

STM32CubeIDE 2.0 release - early heads-up!

Starting from the release in November 2025, STM32CubeIDE and STM32CubeMX will be available exclusively in their standalone versions. STM32CubeMX will no longer be integrated inside STM32CubeIDE. Instead, the two tools will be interoperable in the sam...

Simple HelloWorld ANSI C Project with STM32CubeIDE ?

I'm preparing a basic embedded programming course. I will use some Nucleo boards with CubeIDE. For the bases of C and C++ programming, I also want to use CubeIDE but I didn't found the documentation for configuring STM32CubeIDE to compile a simple AN...

BTrem by Associate II
  • 7638 Views
  • 6 replies
  • 0 kudos

Resolved! Problem on I2S output using HAL

Hi,​I wrote a simplest program (below) to send sine wave data to PCM5102A (DAC) via I2S.​However, I found only L-ch data is valid and R-ch has no data.Analogue (DAC) output of L-ch is somewhat sine wave, but it is sometimes de-formed. And if I look i...

0693W000000XN2BQAW.png
KAJIK.1 by Associate III
  • 5847 Views
  • 5 replies
  • 0 kudos

Resolved! installation of the stm32cubeide

i have got a problem when i download stm32cubeide and install. i have download the file "en.gnu-tools-for-stm32-7-2018-q2-update.20190328-1800.zip" is correct? i have extracted the file, but can not find out the installation file in extract folder. ...

kevin xu by Associate II
  • 2075 Views
  • 3 replies
  • 0 kudos

Wrong download link for STM32CubeIDE

Tried downloading STM32CubeIDE for macOS and Linux (Debian installer). Both of these are not giving the correct download file. It seems to be some kind of source code package to compile a toolchain. Please help!

Include files not added to new source folder.

I created a new source folder in my file stucture, so I have the usual Core and Drivers folders, plus the FreeRTOS folder added by CubeIDE, then I have my App folder. See below.When I compile this, it compiles the three folders the IDE created, but f...

JMill.1 by Associate III
  • 998 Views
  • 1 replies
  • 1 kudos

Build error VFP register argument (STM32F303RE nucleo board)

Hi, I'm trying to use the console in CubeIDE with my STM32F303RE nucleo board and use printf(). For this, I chose an empty project, not STMCube. In the tool settings, I set floating-point unit to none and Floating-point ABI to Software implementation...

JamB by Associate
  • 934 Views
  • 0 replies
  • 0 kudos