2023-12-13 08:11 PM
in debugging mode the values of variables gets corrupted when I check in live expressions. Here corrupted means shows wrong values.
Solved! Go to Solution.
2024-11-06 01:10 AM
@Rim LANDOLSI wrote:The issue has already been reported to STM32CubeIDE development team. An internal ticket ID 168019
See also ticket 175214:
https://community.st.com/t5/stm32cubeide-mcus/live-expressions-bug/m-p/647398/highlight/true#M24957
2024-11-20 06:08 AM
I had the same problem.
I just deleted CubeIDE and reinstalled it again. It Works good.
2024-11-20 06:31 AM - edited 2024-11-20 06:39 AM
Nevermind. The porblem occured again after the next Debug.
It works when you delete all Live Expressions and add them again after starting the debug and resume.
2025-01-10 04:35 AM
This is a significant issue that hasn't been given adequate priority. Despite being reported over a year ago, I am still encountering this problem while using Cube IDE 1.16.1. This issue is causing delays in the debugging process, which in turn hinders product development progress.
2025-01-21 11:41 AM
hi Rim
Is there any update available on this issue?
thanks
paul
2025-02-13 01:44 PM
+1 Please fix this issue.
Best Regards.
2025-02-19 01:43 AM
I am also experiencing this error in CubeIDE version 1.14.0. The live variable sometimes initialize to nonsensicaly high values and I have to stop the debug and start again or reset the board.
2025-02-19 02:32 AM
That's a very old version!
Current is 1.17.0:
https://community.st.com/t5/stm32cubeide-mcus/stm32cubeide-1-17-0-released/td-p/747656
2025-02-19 04:12 AM
I have reported the issue on my current installation, which is 1.17.0, but I have decided to report it in this thread instead of opening a new one. It is noteworthy that this issue is not listed in the errata as having been fixed or as a known bug.
Perhaps @Rim LANDOLSI, you could consider adding it to the list to facilitate future resolution.
Best regards,