2023-11-21 7:29 AM
I use STM32CubeIDE on Linux Ubuntu (and to a lesser extent on MacOS and Windows, but I don't recall having a problem on the last 2 operating systems). About once or twice a day, at random, several of the keys such as <backspace> and <enter> and <delete> stop working. All the alphabetical and number keys work as normal. If I switch to a different application all the keys are working, but when I switch back to Cube the problem continues.
I solve the problem by saving my work, shutting and relaunching Cube. Is this a bug in the application?
Solved! Go to Solution.
2024-02-23 1:16 AM
Hello,
The issue is reported internally to our team (Internal ticket number : 174448) and this will be fixed as soon as possible.
Thanks.
Mahmoud.
2024-02-07 1:35 PM
I've noticed this on Ubuntu also. It seems to occur for me after generating code from the CubeMX view. Restarting STM32CubeIDE resolves the issue, but it is quite annoying.
2024-02-20 11:40 PM
exactly me too.
I met very often while configuration tunings.
select lines and "Edit-Copy" then "Edit-Paste" by mouse operation,
after doing this likely solved for my cases.
it is still bother but easier than restart IDE for me.
2024-02-22 12:46 AM
Hello,
First let me thank you for posting.
Can you provide please the STM32CubeIDE and Ubuntu versions.
Thanks.
Mahmoud.
2024-02-22 1:37 AM
hello,
> Can you provide please the STM32CubeIDE and Ubuntu versions.
STM32CubeIDE version: 1.13.2
Ubuntu 22.04.3 , and also Japanese Language implemented.
I wonder if it may cause or not, though we don't use 2-byte-letter within source code files nor other files in workspace of STM32 project.
in addition, I rarely turn on the IME to Japanese mode with Ubuntu.
(but yes, sure that is there!)
thank you.
2024-02-22 9:17 AM
I'm using Ubuntu 22.04 and STM32CubeIDE 1.14.1.
Thanks.
2024-02-23 1:16 AM
Hello,
The issue is reported internally to our team (Internal ticket number : 174448) and this will be fixed as soon as possible.
Thanks.
Mahmoud.
2024-02-27 3:56 AM
Just in case, the same problem exists on STM32CubeIDE v.1.14.1, Ubuntu 23.10
2024-02-28 4:10 PM
hello,
some additional infos, that I reproduce this issue yesterday.
open *.ioc file then close it and back to the editor view, then control keys wouldn't work. (not edit *.ioc)
-cursor, Ctrl, BackSpace, Del, Enter, or so..
if it's not every time I'm not sure, control keys wouldn't work but only alphabetical keys are work.
-not sure but can be reproduced yesterday.
I guess this sometimes causes build error (or, only mess in the comments), for unexpected strings had put at unexpected location of the source code as say "contaminate" if I may not careful in this situation, and it's the worst.
hope this may help.
BR
2024-04-26 10:28 AM
I have the same problem. My solution is to open the Preferences menu (maybe any other popup window works) and close it by "Apply and Close". I don't do any changes on the Preferences.