cancel
Showing results for 
Search instead for 
Did you mean: 

ITM Debug with SWV H755

tstokes
Associate

I am unable to get ITM debug working via either CubeIDE or Cube programmer. 

 

I have checked the sysclock matches the sysclock configured for the system.

I have tried various limits and auto for the SWV clock.

I have enabled SWV in the debugger config.

In cubeIDE I see no data (port 0 is enabled on the ITM Data Console).

Looking at the log in cubeprogrammer I can see that SWV connects and then disconnects instantly when I click Start on the SWV tab.

tstokes_0-1728309818225.png

Logging and analysing the signals I can see that SWDIO drops at about this time.

 

tstokes_1-1728309947212.png

 

Any ideas?

0 REPLIES 0