cancel
Showing results for 
Search instead for 
Did you mean: 

ST Link Driver Fail / Not Detected in Microsoft Surface Pro 11 Snapdragon (ARM processor laptops)

tnowroz
Associate II

I am using Microsoft Surface Laptop with ARM processor.

Laptop I am using is - Microsoft Surface Pro 13" with Snapdragon X Plus (10 Core) processor.

 

I have installed STM32 CubeIDE and it does install. But while I try to upload code, it fails saying -

"No ST-link Detected" 

 

I can also see that drivers are not installed on device manager. I really do need to work and test on things on the go. I am sure there is a way to work around this. Looking forward to help. Thanks.

3 REPLIES 3
Pavel A.
Super User

What is your ST-Link: standalone like ST-Link v3 MINIE or on-board?

Does Device Manager show anything at all for it?

Hi, 

I have a Nucleo-F411RE board. I do so driver fail at detecting device. 

I downloaded the driver 'en.stsw-link009' but I see it only has x86 and AMD64 titled folders in it. Didn't see anything for ARM.

Your advice is appreciated.

I don't believe ARM is a supported platform currently, not sure where it is on the roadmap.

@STTwo-32 

>>I really do need to work and test on things on the go.

I'd imagine one could find sub $200 x86-64 laptops/desktops if it's mission critical..

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..