cancel
Showing results for 
Search instead for 
Did you mean: 

I want to throw a C file to SD Card and run it from inside the sd card. Is this possible?

KAnahar
Associate III
1 ACCEPTED SOLUTION

Accepted Solutions
Andrew Neil
Evangelist III

No: to do that you would have to have a complete toolchain (compiler, linker, etc) on the Target to compile, link, load, and run the resulting code.

This is the same question as your other thread:

https://community.st.com/s/question/0D53W00001ZZYGdSAP/how-can-i-use-sd-card-with-httpd-server-lwipfatfsethernethttpdsdcard

isn't it?

View solution in original post

3 REPLIES 3
Andrew Neil
Evangelist III

No: to do that you would have to have a complete toolchain (compiler, linker, etc) on the Target to compile, link, load, and run the resulting code.

This is the same question as your other thread:

https://community.st.com/s/question/0D53W00001ZZYGdSAP/how-can-i-use-sd-card-with-httpd-server-lwipfatfsethernethttpdsdcard

isn't it?

but i still searching. i couldnt do anything yet. im stuck :\

then continue in the original thread.

I explained there that you need to have the actual HTML, CSS, JS files themselves on the SD card.

You can mark this thread as answered:

0693W000008y9fZQAQ.png