2024-05-14 04:00 AM - edited 2024-05-14 04:01 AM
This is the first time I use STM32cubeIDE ver 1.15.1 . While using it, there are a few operations that need to be logged in. I already have an account in the practice room at school, but when I log in on my personal laptop, I see a box. "Authentication error manage" dialog as shown below
meanwhile my internet connection is completely normal.
and here is my device information
Device name DESKTOP-4TDRFA4
Processor 11th Gen Intel(R) Core(TM) i5-1135G7 @ 2.40GHz 2.42 GHz
Installed RAM 8.00 GB (7.74 GB usable)
Device ID 996C43EE-CF99-4860-A14A-D9B1A6AE213A
Product ID 00356-24555-97786-AAOEM
System type 64-bit operating system, x64-based processor
Pen and touch No pen or touch input is available for this display
I don't know how to fix the above situation, I hope someone can assist me as soon as possible
It would be better if you guide me with pictures or videos, my English is not very good, please understand
You can contact me via 22200165@student.hcmus.edu.vn
sincerely thank !
Solved! Go to Solution.
2024-05-17 07:02 AM
Dear all,
Seems the issue has been solved please check from your side.
2024-05-14 04:37 AM
I think a lot of people are having this problem today. Come on ST get it fixed. We are trying to do some work here.
2024-05-15 04:58 AM
After wasting almost a full day trying to fix the same issue you encountered, I went through the changelogs and saw that ST started forcing the log in in version 1.13.0 so I installed version 1.12.1 and that seems to work fine.
It's annoying having to use an old version, but well... Hope they fix this soon.
2024-05-15 05:35 AM - edited 2024-05-17 04:33 AM
Same issue With STM32CubeMX V6.11.1
I click yes, and then:
The suggested solution of changing proxy settings doesn't work for me.
now there are at least 8 threads(probably more than 10) about this problem:
https://community.st.com/t5/stm32cubeide-mcus/stm32cubeide-login-issue/td-p/658990
https://community.st.com/t5/stm32-mcus-boards-and-hardware/connection-lost-issue-during-firmware-packages-downloading-in/td-p/674601
https://community.st.com/t5/stm32cubeide-mcus/i-can-t-log-in-myst/td-p/673955
https://community.st.com/t5/stm32cubeide-mcus/stm32cubeide-1-13-2-myst-login-doesn-t-work-with-intermediate/td-p/600164
https://community.st.com/t5/stm32cubemx-mcus/stm32cubemx-version-6-11-1-users-in-my-office-can-t-login-via/td-p/674518
https://community.st.com/t5/stm32cubemx-mcus/help-with-mx/td-p/675509
https://community.st.com/t5/stm32cubemx-mcus/mission-impossible-trying-to-install-the-firmware-package-for/td-p/675385
https://community.st.com/t5/stm32cubeide-mcus/ide-login-issue/td-p/675379
https://community.st.com/t5/stm32cubemx-mcus/mission-impossible-trying-to-install-the-firmware-package-for/td-p/675385
2024-05-16 03:36 AM
Hi Ole1,
Are you able to log in ?
Then, are you able to upgrade to 1.151.1 ?
Regards
2024-05-16 10:41 AM
as said by @Ole1 :
workaround: install CubeIDE 1.12.1
It has no login functionnality and use latest packages.
2024-05-17 03:28 AM
Hello @dnht
First let me thank you for posting.
The issue seems to be linked either to the server or the tool network connection settings.
The possibility of having issue with the server is under investigation.
If you are connected to the internet via a proxy, please follow the steps from the article bellow to set the tool correctly.
How to set the network connection parameters for S... - STMicroelectronics Community
KR,
Ghofrane
2024-05-17 07:02 AM
Dear all,
Seems the issue has been solved please check from your side.
2024-08-16 03:05 PM
I have the same problem:
STM32CUBE IDE 1.16.0 @ win 7 64bit
myST login - nothing happened
Manage Embedded Software Packages - nothing happened
firmware updater -> Check connection - OK
From log:
!MESSAGE Command 'com.st.stm32cube.ide.mcu.ide.command.userAuth.login' failed !STACK 0 org.eclipse.core.commands.ExecutionException: Error executing 'com.st.stm32cube.ide.mcu.ide.command.userAuth.login': java.lang.NullPointerException: Cannot invoke "javax.swing.JComponent.setVisible(boolean)" because "this.webAppContainer" is null
Can you help me? Not possible to continue with work