2023-01-02 1:59 PM
I developed some libs to control a custom LCD.
At the beginning the workspace only had one project, 01_main, and files related to my lcd and driver were located there, later I started another project 02_rtos, so I copied LCD files into new project.
I need to create more projects, libs could be modified from any project, so I create the lib folder, it has the only version of my files, I created this folder with "Link to alternate location"
Everything is working but, My questions:
Is this approach ok? or Is should do something else, please note a want to keep workspace on GitHub, this modify in some way the folder organization approach?
Solved! Go to Solution.
2023-01-04 9:39 AM
@dhs
> they are preferred over git on embedded projects?
They are preferred by large companies with > 100 people working on a project and dedicated IT. Yes, including embedded projects.
They also need more effort to maintain, but are more powerful and flexible, solving dilemmas like yours with ease.
2023-01-02 3:02 PM
> I created this folder with "Link to alternate location"
If it works for you with git, why not.
The "libs" folder can be converted to a git submodule, so it can be shared among other repos/projects.
Other version management systems such as Perforce, Synergy, Clearcase have a different way to maintain and track common files.
2023-01-04 6:00 AM
Hello dhs,
There are at least two approaches to share libs between projects:
1- Share the lib with the project and Link to alternate location created (as you did)
2- Create a static library project. It takes some setup time, but after that it's a more efficient way to manage.
Thanks,
Rim
2023-01-04 9:03 AM
Dear, thank you feedback,
I didn't know about Perforce, Synergy or Clearcase, they are preferred over git on embedded projects?
2023-01-04 9:39 AM
@dhs
> they are preferred over git on embedded projects?
They are preferred by large companies with > 100 people working on a project and dedicated IT. Yes, including embedded projects.
They also need more effort to maintain, but are more powerful and flexible, solving dilemmas like yours with ease.