The message you are trying to access is permanently deleted.
2024-07-20 04:14 AM - edited 2024-07-20 04:15 AM
Hi,
In various ST's example .ioc files, the timer PSC, period, etc, are set with text but not numbers. This will define the numbers to macros in the code. But I can't input text in the CubeIDE. So, is this feature only supported in the standalone version of CubeMX?
Thanks.
Solved! Go to Solution.
2024-07-20 04:19 AM - edited 2024-07-20 04:23 AM
Got it. Just click the gear icon to the right, and select 'no check', then I can input whatever I want.
2024-07-20 04:19 AM - edited 2024-07-20 04:23 AM
Got it. Just click the gear icon to the right, and select 'no check', then I can input whatever I want.