No capture IT triggered
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2024-08-20 4:20 AM
Hi,
Something seems to be wrong with STMCubeIDE Version: 1.16.0 Build: 21983_20240628_1741 (UTC) with an STM32G070RBT6. After generation of the code, the Timer code is like this:
- /**
- * @brief TIM3 Initialization Function
- * @param None
- * @retval None
- */
- static void MX_TIM3_Init(void)
- {
- /* USER CODE BEGIN TIM3_Init 0 */
- // HAL_TIM_IC_DeInit(&htim3); // GDE
- /* USER CODE END TIM3_Init 0 */
- TIM_ClockConfigTypeDef sClockSourceConfig = {0};
- TIM_MasterConfigTypeDef sMasterConfig = {0};
- TIM_IC_InitTypeDef sConfigIC = {0};
- /* USER CODE BEGIN TIM3_Init 1 */
- /* USER CODE END TIM3_Init 1 */
- htim3.Instance = TIM3;
- htim3.Init.Prescaler = 1;
- htim3.Init.CounterMode = TIM_COUNTERMODE_UP;
- htim3.Init.Period = 65535;
- htim3.Init.ClockDivision = TIM_CLOCKDIVISION_DIV1;
- htim3.Init.AutoReloadPreload = TIM_AUTORELOAD_PRELOAD_ENABLE;
- if (HAL_TIM_Base_Init(&htim3) != HAL_OK)
- {
- Error_Handler();
- }
- sClockSourceConfig.ClockSource = TIM_CLOCKSOURCE_INTERNAL;
- if (HAL_TIM_ConfigClockSource(&htim3, &sClockSourceConfig) != HAL_OK)
- {
- Error_Handler();
- }
- if (HAL_TIM_IC_Init(&htim3) != HAL_OK)
- {
- Error_Handler();
- }
- sMasterConfig.MasterOutputTrigger = TIM_TRGO_RESET;
- sMasterConfig.MasterSlaveMode = TIM_MASTERSLAVEMODE_DISABLE;
- if (HAL_TIMEx_MasterConfigSynchronization(&htim3, &sMasterConfig) != HAL_OK)
- {
- Error_Handler();
- }
- sConfigIC.ICPolarity = TIM_INPUTCHANNELPOLARITY_RISING;
- sConfigIC.ICSelection = TIM_ICSELECTION_DIRECTTI;
- sConfigIC.ICPrescaler = TIM_ICPSC_DIV1;
- sConfigIC.ICFilter = 0;
- if (HAL_TIM_IC_ConfigChannel(&htim3, &sConfigIC, TIM_CHANNEL_1) != HAL_OK)
- {
- Error_Handler();
- }
- /* USER CODE BEGIN TIM3_Init 2 */
- /* USER CODE END TIM3_Init 2 */
- }
When we call HAL_TIM_IC_Init() function, the htim->State is already set to HAL_TIM_STATE_READY instead of HAL_TIM_STATE_RESET, so HAL_TIM_IC_MspInit(htim) is never called.
So the interrupt is not triggered, HAL_TIM_IC_CaptureCallback() is never called too.
Is my analysis right?
Solved! Go to Solution.
Accepted Solutions
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2024-08-21 4:15 AM
I've solved the problem.
The MX_NVIC_Init() function called in main does the same thing as the HAL_TIM_IC_MspInit() function, but without testing htim->State.
With the correct NVIC initialization:
/* TIM3_IRQn interrupt configuration */
HAL_NVIC_SetPriority(TIM3_IRQn, 0, 0);
HAL_NVIC_EnableIRQ(TIM3_IRQn);
Now it's OK.
Thanks for your help.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2024-08-20 5:32 AM - edited ‎2024-08-20 5:36 AM
htim3 is zero-initialized at the start, which sets its state to HAL_TIM_STATE_RESET. Must be something else going on here. Perhaps show your full main.c code. You could set a watchpoint on htim->State to see where it's being modified.
Edit: Oh, I see it gets set to READY in HAL_TIM_Base_Init. Yeah, you may be right. Sorry for noise.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2024-08-21 4:15 AM
I've solved the problem.
The MX_NVIC_Init() function called in main does the same thing as the HAL_TIM_IC_MspInit() function, but without testing htim->State.
With the correct NVIC initialization:
/* TIM3_IRQn interrupt configuration */
HAL_NVIC_SetPriority(TIM3_IRQn, 0, 0);
HAL_NVIC_EnableIRQ(TIM3_IRQn);
Now it's OK.
Thanks for your help.