2025-01-08 11:12 AM
I can't login into ST to download packages via CubeMX/CubeIDE. The wheel turns forever, no matter what proxy settings I choose. The pack downloader works - I just can't log into ST which is a pitty.
Which url does my corporate IT whitelist?
See similar issue here: Solved: Unable to login to ST account in STM32CubeIDE - STMicroelectronics Community
Thanks,
Jan
Solved! Go to Solution.
2025-03-19 1:21 AM
Dear @JKapp.1, @Billy Owen, @KDJEM.1,
Thank you for the help. We have been informed by our Regional FAE that case 00223403 is closed by customer @JKapp.1 on 17 January 2025, and no more unusual behavior has been observed. I propose to close the case here as well. Feel free to contact us for any further escalations related to this case.
Regards,
STOne-32.
2025-01-09 12:11 AM - edited 2025-01-09 12:15 AM
Hello @JKapp.1
Could you please try to clear your browser cache as mentioned by @Laurids_PETERSEN in this post: "Solved: ST community login issue - STMicroelectronics Community".
May be you encountered an authentication problem while using STM32CubeIDE, you need to set your connection parameters and to use offline mode as mentioned in this link: How to set the network connection parameters for S... - STMicroelectronics Community.
If you are still having issues, please let me know.
Thank you.
Kaouthar
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2025-01-09 1:21 AM - edited 2025-01-09 1:31 AM
Hi @KDJEM.1
Which cache do I have to clear? I can login with both browsers, Chrome and Edge, but not via CubeMX/CubeIDE - which browser is used there to login?
I have set the proxy settings correctly "check connection" is green:
Nevertheless, I can't login to myST.
Thanks
EDIT: Check connection only works in CubeMX, but not in CubeIDE - same proxy settings wtf?
EDIT2: this is from CubeIDE:
But upgrading the package index works
2025-01-09 7:59 AM
Hi @JKapp.1
This post has been escalated to the ST Online Support Team for additional assistance. We'll contact you directly.
Regards,
Billy
2025-03-19 1:21 AM
Dear @JKapp.1, @Billy Owen, @KDJEM.1,
Thank you for the help. We have been informed by our Regional FAE that case 00223403 is closed by customer @JKapp.1 on 17 January 2025, and no more unusual behavior has been observed. I propose to close the case here as well. Feel free to contact us for any further escalations related to this case.
Regards,
STOne-32.