cancel
Showing results for 
Search instead for 
Did you mean: 

Error : make: *** No rule to make target.....

DYann.1
Senior II

Hello,

Someone sends me a project but when I open it on my PC I encounter the following error :

make: *** No rule to make target 'C:/Users/ghithab/STM32Cube/Repository/STM32Cube_FW_L5_V1.5.1/Middlewares/Third_Party/FatFs/src/option/ccsbcs.c', needed by 'Middlewares/FatFs/ccsbcs.o'. Stop. FatFs_uSD_Standalone C/C++ Problem

 

Do you know how to fix this problem ? However in my directory I have the file in question :

DYann1_0-1732093495210.png

This probably comes from the configuration path but I only see points....

DYann1_1-1732093593679.png

How i can see the full path instead of the....

DYann1_3-1732093643053.png

Thank you for your helps

Regards

4 REPLIES 4
SofLit
ST Employee

Hello,

Was this file added to the project:

SofLit_0-1732107282903.png

-> This is an example from https://github.com/STMicroelectronics/STM32CubeL5/tree/master/Projects/STM32L562E-DK/Applications/FatFs/FatFs_uSD_Standalone

Otherwise, if possible to share with us your project. If not possible to share it in public send it to me in private.

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.

Hi,

Thank you for your answer, Can I send you privately ? Please

Yes

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.

Yes I have this file in my Projet

DYann1_1-1732113419321.png

So Where is the problem ? The Path configuration probably ?