2019-05-21 07:31 PM
I am trying to debug my code, but it just ain't working the way it's working in e.g. the STM32CubeIDE intro-video on Youtube; I'm getting "No source available for main()", instead of Eclipse displaying where in the code it's actually at.
I haven't changed any of the default-settings, other than where my workspace is and yes, I have build a debug-version instead of release-version and yes, I do see "-g3" - flag enabled in the compilation-console.
How do I fix this?
2019-05-21 07:41 PM
Apparently the problem was that I had both the "release"-executable and the "debug"-executable there and Eclipse insisted on using the wrong one.
2019-05-24 12:20 AM
Hi,
I've the same problem "No source available for "main() at 0x800559e" with Atollic TrueSTUDIO® for STM32, Built on Eclipse Neon.1a. Version: 9.3.0
Any suggestion ?
2020-02-15 03:22 PM
Click Debug button, Debug Configurations.
Choose STM32 Cortex-M C/C++ Application, Your application name if exists, if not double click "STM32 Cortex-M C/C++ Application" and create one.
Browse for correct elf file for C/C++ Application: Debug/my_meaga_app.elf
2021-04-11 01:56 AM
Hi
It is possible that you have left the BOOT0 pin on your micro-controller floating. To load the program from flash it has to be tied to ground.
Regards,
2021-04-11 04:56 AM
That's because you're debugging with a release build.
Go to debug profiles, and ensure that it's getting the debug build.
Also enabling autobuild is a good idea.
2021-05-13 11:56 AM
I had the same problem and here is the solution:
Project => Properties => C/C++ Build (Tree) => Settings => Tool Settings (Tab) => MCU GCC Compiler (Tree) => Optimization
In the “Optimization Level�? list box field I selected “Optimize for Debug (-Og)"
Project => Properties => C/C++ Build (Tree) => Settings => Tool Settings (Tab) => MCU GCC Compiler (Tree) => Debugging
In the “Debug Level�? list box field I selected “Maximum (-g3)�?
2021-10-14 09:12 AM
Thanks, man!
2022-03-31 02:22 PM
thanks AGrun.1 this worked for me
appreciate you putting it out there.
2024-02-07 11:22 AM
Thank you @AGrun.1
Hi @anonymous.8 , does the solution given by @AGrun.1 is also working for you or you still have issues ?
Best regards