cancel
Showing results for 
Search instead for 
Did you mean: 

Custom linker won't compile

MBeau.1
Associate

I'm trying to reserve space in RAM for emulated eeprom. I can read and write fine, however when I try to modify the linker it won't compile.

The added user section

/* Specify the memory areas */
MEMORY
{
  FLASH (rx)      : ORIGIN = 0x08000000, LENGTH = 96K
  USER_DATA (rwx) : ORIGIN = ORIGIN(FLASH) + LENGTH(FLASH)‬‬, LENGTH = 32K
  RAM (xrw)       : ORIGIN = 0x20000000, LENGTH = 8K
  MEMORY_B1 (rx)  : ORIGIN = 0x60000000, LENGTH = 0K
}

Howerver when trying to compile it says «invalid character» at the line of the new section in the linker script:

c:\st\stm32cubeide_1.3.0\stm32cubeide\plugins\com.st.stm32cube.ide.mcu.externaltools.gnu-tools-for-stm32.7-2018-q2-update.win32_1.0.0.201904181610\tools\arm-none-eabi\bin\ld.exe:../stm32_flash.ld:48: ignoring invalid character `\342' in expression

c:\st\stm32cubeide_1.3.0\stm32cubeide\plugins\com.st.stm32cube.ide.mcu.externaltools.gnu-tools-for-stm32.7-2018-q2-update.win32_1.0.0.201904181610\tools\arm-none-eabi\bin\ld.exe:../stm32_flash.ld:48: ignoring invalid character `\200' in expression

attempt to open c:/st/stm32cubeide_1.3.0/stm32cubeide/plugins/com.st.stm32cube.ide.mcu.externaltools.gnu-tools-for-stm32.7-2018-q2-update.win32_1.0.0.201904181610/tools/bin/../lib/gcc/arm-none-eabi/7.3.1/thumb/v7-m\libm.a failed

c:\st\stm32cubeide_1.3.0\stm32cubeide\plugins\com.st.stm32cube.ide.mcu.externaltools.gnu-tools-for-stm32.7-2018-q2-update.win32_1.0.0.201904181610\tools\arm-none-eabi\bin\ld.exe:../stm32_flash.ld:48: ignoring invalid character `\254' in expression

c:\st\stm32cubeide_1.3.0\stm32cubeide\plugins\com.st.stm32cube.ide.mcu.externaltools.gnu-tools-for-stm32.7-2018-q2-update.win32_1.0.0.201904181610\tools\arm-none-eabi\bin\ld.exe:../stm32_flash.ld:48: ignoring invalid character `\342' in expression

c:\st\stm32cubeide_1.3.0\stm32cubeide\plugins\com.st.stm32cube.ide.mcu.externaltools.gnu-tools-for-stm32.7-2018-q2-update.win32_1.0.0.201904181610\tools\arm-none-eabi\bin\ld.exe:../stm32_flash.ld:48: ignoring invalid character `\200' in expression

This discussion is locked. Please start a new topic to ask your question.
1 ACCEPTED SOLUTION

Accepted Solutions
TDK
Guru

You have unicode characters in your script which should be strictly ASCII.

Delete the line it's complaining about and retype it on the keyboard. Don't copy/paste.

If you feel a post has answered your question, please click "Accept as Solution".

View solution in original post

3 REPLIES 3
TDK
Guru

You have unicode characters in your script which should be strictly ASCII.

Delete the line it's complaining about and retype it on the keyboard. Don't copy/paste.

If you feel a post has answered your question, please click "Accept as Solution".
MBeau.1
Associate

It did the trick, I used a different editor as well.

Pasting via generic Notepad app can strip formatting.

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..