cancel
Showing results for 
Search instead for 
Did you mean: 

Compiler / Linker Broken in CubeIDE

matt-crc
Senior III

The CubeIDE linker doesn't seem to work properly... Any help would be greatly appreciated.  ST Employee help?????

1- In the UserStartup.c, I call lv_init();

2- After compiling, it says it cannot find lv_init()

3- I see that the file lv_init.c file got compiled (lv_init() is defined in that file) - the object file was created lv_init.o

4- It seems the linker cannot find that file....

Is there a limitation on the number of files the linker can handle?

 

mattcrc_0-1743108440574.png

 

11 REPLIES 11
Pavel A.
Super User

The linker in the toolchain of CubeIDE has no limitations. The file lv_init.c indeed seems to be compiled. Try to double check why  lv_init.o is not linked or the required functions in it are not found. Bug in the linker is unlikely. Bugs of this kind usually occur between the chair and keyboard ))

Hi @Pavel A. 

I'd be really happy if the bug is between the chair and keyboard, but things seem to be pointing to the compiler.  Also, in the pre-compiler, there seems to be a problem with the includes.

In one file (early on in the compile), it has no problem finding the "#include "lvgl.h" file.  as the 6 min compilation continues, files compiled later with the same "#include lvgl.h"  generates and error: "Cannot find include file"

If I change the "#include "lvgl.h" to the real path, and not using the include search path, then the file compiles... To me this looks and sounds like a compiler limitation....  

 

Also, there seems to be a limitation to the number of SRC directories defined in CubeIDE  (max 10).  Most were autogenerated by CubeMX.  I know this is a large compile and we are definitely pushing the limits of the IDE.

 

Pavel A.
Super User

What is the CubeIDE version and STM32? Is any antivirus (or worse) installed? Are you by chance low on disk space?

 

 

matt-crc
Senior III

Hi @Pavel A. 

The machine that I'm using is a Dell Precision 3660 with 12th gen processor, and 64gb mem.  Over 1.2TB free on disk

STM32CubeIDE is version 1.18.0, Build 24413_20250227_1633

No antivirus installed, 

Andrew Neil
Super User

@matt-crc wrote:

3- I see that the file lv_init.c file got compiled (lv_init() is defined in that file)


Is it?

You haven't shown that

A complex system that works is invariably found to have evolved from a simple system that worked.
A complex system designed from scratch never works and cannot be patched up to make it work.

 

@Andrew Neil 

mattcrc_1-1743121180939.png

line 172

/**
 * @file lv_init.c
 *
 */

/*********************
 *      INCLUDES
 *********************/
#include "misc/lv_timer_private.h"
#include "misc/lv_profiler_builtin_private.h"
#include "misc/lv_anim_private.h"
#include "draw/lv_image_decoder_private.h"
#include "draw/lv_draw_buf_private.h"
#include "core/lv_refr_private.h"
#include "core/lv_obj_style_private.h"
#include "core/lv_group_private.h"
#include "lv_init.h"
#include "core/lv_global.h"
#include "core/lv_obj.h"
#include "display/lv_display_private.h"
#include "indev/lv_indev_private.h"
#include "layouts/lv_layout_private.h"
#include "libs/bin_decoder/lv_bin_decoder.h"
#include "libs/bmp/lv_bmp.h"
#include "libs/ffmpeg/lv_ffmpeg.h"
#include "libs/freetype/lv_freetype.h"
#include "libs/fsdrv/lv_fsdrv.h"
#include "libs/gif/lv_gif.h"
#include "libs/tjpgd/lv_tjpgd.h"
#include "libs/libjpeg_turbo/lv_libjpeg_turbo.h"
#include "libs/lodepng/lv_lodepng.h"
#include "libs/libpng/lv_libpng.h"
#include "libs/tiny_ttf/lv_tiny_ttf.h"
#include "draw/lv_draw.h"
#include "misc/lv_async.h"
#include "misc/lv_fs_private.h"
#include "widgets/span/lv_span.h"
#include "themes/simple/lv_theme_simple.h"
#include "misc/lv_fs.h"
#include "osal/lv_os_private.h"
#include "others/sysmon/lv_sysmon_private.h"
#include "others/xml/lv_xml.h"

#if LV_USE_SVG
    #include "libs/svg/lv_svg_decoder.h"
#endif

#if LV_USE_NEMA_GFX
    #include "draw/nema_gfx/lv_draw_nema_gfx.h"
#endif
#if LV_USE_DRAW_VGLITE
    #include "draw/nxp/vglite/lv_draw_vglite.h"
#endif
#if LV_USE_PXP
    #if LV_USE_DRAW_PXP || LV_USE_ROTATE_PXP
        #include "draw/nxp/pxp/lv_draw_pxp.h"
    #endif
#endif
#if LV_USE_DRAW_G2D
    #include "draw/nxp/g2d/lv_draw_g2d.h"
#endif
#if LV_USE_DRAW_DAVE2D
    #include "draw/renesas/dave2d/lv_draw_dave2d.h"
#endif
#if LV_USE_DRAW_SDL
    #include "draw/sdl/lv_draw_sdl.h"
#endif
#if LV_USE_DRAW_VG_LITE
    #include "draw/vg_lite/lv_draw_vg_lite.h"
#endif
#if LV_USE_DRAW_DMA2D
    #include "draw/dma2d/lv_draw_dma2d.h"
#endif
#if LV_USE_DRAW_OPENGLES
    #include "draw/opengles/lv_draw_opengles.h"
#endif
#if LV_USE_WINDOWS
    #include "drivers/windows/lv_windows_context.h"
#endif
#if LV_USE_UEFI
    #include "drivers/uefi/lv_uefi_context.h"
#endif
#if LV_USE_EVDEV
    #include "drivers/evdev/lv_evdev_private.h"
#endif

/*********************
 *      DEFINES
 *********************/
#define lv_initialized  LV_GLOBAL_DEFAULT()->inited
#define lv_deinit_in_progress  LV_GLOBAL_DEFAULT()->deinit_in_progress

/**********************
 *      TYPEDEFS
 **********************/

/**********************
 *  STATIC PROTOTYPES
 **********************/

/**********************
 *  STATIC VARIABLES
 **********************/
#if LV_ENABLE_GLOBAL_CUSTOM == 0
    lv_global_t lv_global;
#endif

/**********************
 *      MACROS
 **********************/

#ifndef LV_GLOBAL_INIT
    #define LV_GLOBAL_INIT(__GLOBAL_PTR)    lv_global_init((lv_global_t *)(__GLOBAL_PTR))
#endif

/**********************
 *   GLOBAL FUNCTIONS
 **********************/
static inline void lv_global_init(lv_global_t * global)
{
    LV_ASSERT_NULL(global);

    if(global == NULL) {
        LV_LOG_ERROR("lv_global cannot be null");
        return;
    }

    lv_memzero(global, sizeof(lv_global_t));

    lv_ll_init(&(global->disp_ll), sizeof(lv_display_t));
    lv_ll_init(&(global->indev_ll), sizeof(lv_indev_t));

    global->memory_zero = ZERO_MEM_SENTINEL;
    global->style_refresh = true;
    global->layout_count = LV_LAYOUT_LAST;
    global->style_last_custom_prop_id = (uint32_t)LV_STYLE_LAST_BUILT_IN_PROP;
    global->event_last_register_id = LV_EVENT_LAST;
    lv_rand_set_seed(0x1234ABCD);

#ifdef LV_LOG_PRINT_CB
    void LV_LOG_PRINT_CB(lv_log_level_t, const char * txt);
    global->custom_log_print_cb = LV_LOG_PRINT_CB;
#endif

#if defined(LV_DRAW_SW_SHADOW_CACHE_SIZE) && LV_DRAW_SW_SHADOW_CACHE_SIZE > 0
    global->sw_shadow_cache.cache_size = -1;
    global->sw_shadow_cache.cache_r = -1;
#endif
}

static inline void lv_cleanup_devices(lv_global_t * global)
{
    LV_ASSERT_NULL(global);

    if(global) {
        /* cleanup indev and display */
        lv_ll_clear_custom(&(global->indev_ll), (void (*)(void *)) lv_indev_delete);
        lv_ll_clear_custom(&(global->disp_ll), (void (*)(void *)) lv_display_delete);
    }
}

bool lv_is_initialized(void)
{
#if LV_ENABLE_GLOBAL_CUSTOM
    if(LV_GLOBAL_DEFAULT()) return lv_initialized;
    else return false;
#else
    return lv_initialized;
#endif
}

void lv_init(void)
{
    /*First initialize Garbage Collection if needed*/
#ifdef LV_GC_INIT
    LV_GC_INIT();
#endif

    /*Do nothing if already initialized*/
    if(lv_initialized) {
        LV_LOG_WARN("lv_init: already initialized");
        return;
    }

    LV_LOG_INFO("begin");

    /*Initialize members of static variable lv_global */
    LV_GLOBAL_INIT(LV_GLOBAL_DEFAULT());

    lv_mem_init();

    lv_draw_buf_init_handlers();

#if LV_USE_SPAN != 0
    lv_span_stack_init();
#endif

#if LV_USE_PROFILER && LV_USE_PROFILER_BUILTIN
    lv_profiler_builtin_config_t profiler_config;
    lv_profiler_builtin_config_init(&profiler_config);
    lv_profiler_builtin_init(&profiler_config);
#endif

    lv_os_init();

    lv_timer_core_init();

    lv_fs_init();

    lv_layout_init();

    lv_anim_core_init();

    lv_group_init();

#if LV_USE_FREETYPE
    /* Since the drawing unit needs to register the freetype event,
     * initialize the freetype module first
     */
    lv_freetype_init(LV_FREETYPE_CACHE_FT_GLYPH_CNT);
#endif

    lv_draw_init();

#if LV_USE_DRAW_SW
    lv_draw_sw_init();
#endif

#if LV_USE_NEMA_GFX
    lv_draw_nema_gfx_init();
#endif

#if LV_USE_DRAW_VGLITE
    lv_draw_vglite_init();
#endif

#if LV_USE_PXP
#if LV_USE_DRAW_PXP || LV_USE_ROTATE_PXP
    lv_draw_pxp_init();
#endif
#endif

#if LV_USE_DRAW_G2D
    lv_draw_g2d_init();
#endif

#if LV_USE_DRAW_DAVE2D
    lv_draw_dave2d_init();
#endif

#if LV_USE_DRAW_SDL
    lv_draw_sdl_init();
#endif

#if LV_USE_DRAW_DMA2D
    lv_draw_dma2d_init();
#endif

#if LV_USE_DRAW_OPENGLES
    lv_draw_opengles_init();
#endif

#if LV_USE_WINDOWS
    lv_windows_platform_init();
#endif

#if LV_USE_UEFI
    lv_uefi_platform_init();
#endif

    lv_obj_style_init();

    /*Initialize the screen refresh system*/
    lv_refr_init();

#if LV_USE_SYSMON
    lv_sysmon_builtin_init();
#endif

    lv_image_decoder_init(LV_CACHE_DEF_SIZE, LV_IMAGE_HEADER_CACHE_DEF_CNT);
    lv_bin_decoder_init();  /*LVGL built-in binary image decoder*/

#if LV_USE_DRAW_VG_LITE
    lv_draw_vg_lite_init();
#endif

    /*Test if the IDE has UTF-8 encoding*/
    const char * txt = "Á";

    uint8_t * txt_u8 = (uint8_t *)txt;
    if(txt_u8[0] != 0xc3 || txt_u8[1] != 0x81 || txt_u8[2] != 0x00) {
        LV_LOG_WARN("The strings have no UTF-8 encoding. Non-ASCII characters won't be displayed.");
    }

    uint32_t endianness_test = 0x11223344;
    uint8_t * endianness_test_p = (uint8_t *) &endianness_test;
    bool big_endian = endianness_test_p[0] == 0x11;

    if(big_endian) {
        LV_ASSERT_MSG(LV_BIG_ENDIAN_SYSTEM == 1,
                      "It's a big endian system but LV_BIG_ENDIAN_SYSTEM is not enabled in lv_conf.h");
    }
    else {
        LV_ASSERT_MSG(LV_BIG_ENDIAN_SYSTEM == 0,
                      "It's a little endian system but LV_BIG_ENDIAN_SYSTEM is enabled in lv_conf.h");
    }

#if LV_USE_ASSERT_MEM_INTEGRITY
    LV_LOG_WARN("Memory integrity checks are enabled via LV_USE_ASSERT_MEM_INTEGRITY which makes LVGL much slower");
#endif

#if LV_USE_ASSERT_OBJ
    LV_LOG_WARN("Object sanity checks are enabled via LV_USE_ASSERT_OBJ which makes LVGL much slower");
#endif

#if LV_USE_ASSERT_STYLE
    LV_LOG_WARN("Style sanity checks are enabled that uses more RAM");
#endif

#if LV_LOG_LEVEL == LV_LOG_LEVEL_TRACE
    LV_LOG_WARN("Log level is set to 'Trace' which makes LVGL much slower");
#endif

#if LV_USE_FS_FATFS != '\0'
    lv_fs_fatfs_init();
#endif

#if LV_USE_FS_STDIO != '\0'
    lv_fs_stdio_init();
#endif

#if LV_USE_FS_POSIX != '\0'
    lv_fs_posix_init();
#endif

#if LV_USE_FS_WIN32 != '\0'
    lv_fs_win32_init();
#endif

#if LV_USE_FS_MEMFS
    lv_fs_memfs_init();
#endif

#if LV_USE_FS_LITTLEFS
    lv_fs_littlefs_init();
#endif

#if LV_USE_FS_ARDUINO_ESP_LITTLEFS
    lv_fs_arduino_esp_littlefs_init();
#endif

#if LV_USE_FS_ARDUINO_SD
    lv_fs_arduino_sd_init();
#endif

#if LV_USE_FS_UEFI
    lv_fs_uefi_init();
#endif

#if LV_USE_LODEPNG
    lv_lodepng_init();
#endif

#if LV_USE_LIBPNG
    lv_libpng_init();
#endif

#if LV_USE_TJPGD
    lv_tjpgd_init();
#endif

#if LV_USE_LIBJPEG_TURBO
    lv_libjpeg_turbo_init();
#endif

#if LV_USE_BMP
    lv_bmp_init();
#endif

#if LV_USE_SVG
    lv_svg_decoder_init();
#endif

    /*Make FFMPEG last because the last converter will be checked first and
     *it's superior to any other */
#if LV_USE_FFMPEG
    lv_ffmpeg_init();
#endif

#if LV_USE_XML
    lv_xml_init();
#endif

    lv_initialized = true;

    LV_LOG_TRACE("finished");
}

void lv_deinit(void)
{
    /*Do nothing if already deinit*/
    if(!lv_initialized) {
        LV_LOG_WARN("lv_deinit: already deinit!");
        return;
    }

    if(lv_deinit_in_progress) return;

    lv_deinit_in_progress = true;

#if LV_USE_SYSMON
    lv_sysmon_builtin_deinit();
#endif

    lv_display_set_default(NULL);

    lv_cleanup_devices(LV_GLOBAL_DEFAULT());

#if LV_USE_EVDEV
    lv_evdev_deinit();
#endif

#if LV_USE_SPAN != 0
    lv_span_stack_deinit();
#endif

#if LV_USE_FREETYPE
    lv_freetype_uninit();
#endif

#if LV_USE_THEME_DEFAULT
    lv_theme_default_deinit();
#endif

#if LV_USE_THEME_SIMPLE
    lv_theme_simple_deinit();
#endif

#if LV_USE_THEME_MONO
    lv_theme_mono_deinit();
#endif

    lv_image_decoder_deinit();

    lv_refr_deinit();

    lv_obj_style_deinit();

#if LV_USE_UEFI
    lv_uefi_platform_deinit();
#endif

#if LV_USE_PXP
#if LV_USE_DRAW_PXP || LV_USE_ROTATE_PXP
    lv_draw_pxp_deinit();
#endif
#endif

#if LV_USE_DRAW_VGLITE
    lv_draw_vglite_deinit();
#endif

#if LV_USE_DRAW_G2D
    lv_draw_g2d_deinit();
#endif

#if LV_USE_DRAW_VG_LITE
    lv_draw_vg_lite_deinit();
#endif

#if LV_USE_DRAW_DMA2D
    lv_draw_dma2d_deinit();
#endif

#if LV_USE_DRAW_OPENGLES
    lv_draw_opengles_deinit();
#endif

#if LV_USE_DRAW_SW
    lv_draw_sw_deinit();
#endif

    lv_draw_deinit();

    lv_group_deinit();

    lv_anim_core_deinit();

    lv_layout_deinit();

    lv_fs_deinit();

    lv_timer_core_deinit();

#if LV_USE_PROFILER && LV_USE_PROFILER_BUILTIN
    lv_profiler_builtin_uninit();
#endif

#if LV_USE_OBJ_ID && LV_USE_OBJ_ID_BUILTIN
    lv_objid_builtin_destroy();
#endif

    lv_mem_deinit();

    lv_initialized = false;

    LV_LOG_INFO("lv_deinit done");

#if LV_USE_LOG
    lv_log_register_print_cb(NULL);
#endif

}

/**********************
 *   STATIC FUNCTIONS
 **********************/

 

TDK
Super User

Can you copy the full contents of the Console tab from a clean build into a text file and include it here?

If you feel a post has answered your question, please click "Accept as Solution".
matt-crc
Senior III

Hi @TDK 

Funny that you suggested that... I've been trying to do that for days....  Unfortunately I can't figure out how to capture the entire console.  It scrolls past the console buffer size, so I can only get the bottom 1/3 of the project.  Is there a setting that increases the buffer size?  I see there were some warnings when compiling but I haven't been able to scroll back to see them.

 

BTW, I finally reduced the size of LVGL component by unconfiguring a lot of options and finally got a working executable.  I was going to run it this afternoon to see how it runs on the hardware.

matt-crc
Senior III

This is all that the console can capture