2024-09-04 09:04 AM
Hi,
Stm32cubeide keeps crashing anytime I try to create a new stm32 project. The program makes it to the board select screen then crashes. I’m on an Intel MacBook Pro running Sonoma 14.6.1. I have Stm32cubeide updated to 1.16.0. Does anyone have any ideas how I can resolve the issue? Below is a snippet from the crash report. I've also attached the full report as well. Any help would be greatly appreciated. Thanks
Crashed Thread: 0 Dispatch queue: com.apple.main-thread
Exception Type: EXC_BAD_ACCESS (SIGABRT)
Exception Codes: KERN_INVALID_ADDRESS at 0x00007ff700000000
Exception Codes: 0x0000000000000001, 0x00007ff700000000
Termination Reason: Namespace SIGNAL, Code 6 Abort trap: 6
Terminating Process: stm32cubeide [2937]
VM Region Info: 0x7ff700000000 is not in any region. Bytes after previous region: 319564021761 Bytes before following region: 3146084352
REGION TYPE START - END [ VSIZE] PRT/MAX SHRMOD REGION DETAIL
MALLOC_SMALL 7fac98000000-7fac98800000 [ 8192K] rw-/rwx SM=PRV
---> GAP OF 0x4b23057000 BYTES
Stack Guard 7ff7bb857000-7ff7bf057000 [ 56.0M] ---/rwx SM=NUL
Application Specific Information:
abort() called
Thread 0 Crashed:: Dispatch queue: com.apple.main-thread