cancel
Showing results for 
Search instead for 
Did you mean: 

After upgrade of STM32CubeIDE to 1.16.0 IDE screen messed up

eBirdman
Senior II

Hello, after I upgraded my ubuntu  STM32CubeIDE from 1.14.0 to 1.16.0 I am getting the IDE menus messed up, menu fonts messed up and some portions of the screen are black. Previous version 1.14.0 (and respective toolchain) did not have any problem.

My laptop is System76 with Ubuntu 22.04.4.LTS , Window system Wayland, Gnome v. 42.9, all packages are the latest. All the latest Ubuntu packages were updated and I still used IDE v. 1.14.0 - everything was fine. Only after the IDE upgrade to 1.16.0 (nothing else was changed in the system) the screen got messed up. After yet a repeated re-installation (1st delete all previously installed versions of IDE, then re-install) of V. 1.16.0  IDE looked fine but after the laptop was suspended and woke up, the same problem with screen repeated. My working preferences were imported - didn't help. I switched the IDE theme setting to another theme style in order to update the IDE windows , restarted - didn't help. Screenshot is attached.

Please help - our project stuck.

0 REPLIES 0