cancel
Showing results for 
Search instead for 
Did you mean: 

Crashing when creating a new STM32 Project

namesjames
Associate

Hi,

Stm32cubeide keeps crashing anytime I try to create a new stm32 project. The program makes it to the board select screen then crashes. I’m on an Intel MacBook Pro running Sonoma 14.6.1. I have Stm32cubeide updated to 1.16.0. Does anyone have any ideas how I can resolve the issue? Below is a snippet from the crash report. I've also attached the full report as well. Any help would be greatly appreciated. Thanks

 

Crashed Thread:        0  Dispatch queue: com.apple.main-thread

 

Exception Type:        EXC_BAD_ACCESS (SIGABRT)

Exception Codes:       KERN_INVALID_ADDRESS at 0x00007ff700000000

Exception Codes:       0x0000000000000001, 0x00007ff700000000

 

Termination Reason:    Namespace SIGNAL, Code 6 Abort trap: 6

Terminating Process:   stm32cubeide [2937]

 

VM Region Info: 0x7ff700000000 is not in any region.  Bytes after previous region: 319564021761  Bytes before following region: 3146084352

      REGION TYPE                    START - END         [ VSIZE] PRT/MAX SHRMOD  REGION DETAIL

      MALLOC_SMALL             7fac98000000-7fac98800000 [ 8192K] rw-/rwx SM=PRV 

--->  GAP OF 0x4b23057000 BYTES

      Stack Guard              7ff7bb857000-7ff7bf057000 [ 56.0M] ---/rwx SM=NUL 

 

Application Specific Information:

abort() called

Thread 0 Crashed::  Dispatch queue: com.apple.main-thread

0 REPLIES 0