Compiling a project generated by CubeIde with FreeRtos, None timer on systick and LL driver only end with error
Options
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2020-06-22 7:47 AM
In a particular time critical application, I'd like to use the LL driver only, FreeRtos and, to preserve an hw resouce, I've selected "none" in SystemCore->Sys->TimeBaseSource.
Trying to compile the project generated in this way, I get "fatal error: stm32g0xx_hal.h: No such file or directory", even if I don't use hal at all.
If I delete the file stm32g0xx_hal_gpio.c from source, the project compile correctly, but if I rebuild the project from the ioc, the file is created again and the error is the same.
Step to reproduce the problem:
- Create a new project for STM32G070 microcontroller
- In the ioc file enable CMSIS_V1 in Middleware->freertos configuration
- In the ioc file set SystemCore->Sys->TimeBaseSource to "none"
- In the ioc file set Project Manager -> Advanced Settings -> RCC to LL
- Generate the code
- Try to compile
STM32CubeG0 Firmware Package V1.3.0
STM32CubeIDE Version: 1.3.1 Build: 6291_20200406_0752 (UTC)
Thank You in advance
Paolo
Labels:
- Labels:
-
FreeRTOS
-
STM32CubeIDE
-
STM32G0 Series
This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0