2025-01-08 01:02 AM
Hi evryone,
I'm trying to do some work on the stm32 L552ZE-Q and I'm trying to launch some demo projects available but once I've imported the porject in the IDE I can't build the project. I have that error:
and I also got a warning but I don't find why it is here:
And the build button is inaccessible:
Thank you for your help!
2025-01-08 01:31 AM
Hello @_Louis_ ,
It seems you are using the "Copy into workspace" option ?
In this case, you have this known limitation which is listed in the STM32CubeIDE:STM32CubeIDE errata 1.17.x - stm32mcu
68184 | Hierarchical projects cannot be imported with the option Copy into workspace. |
2025-01-08 05:59 PM
Hi Imen,
I've try to import the file via different methods:
And every method fail to build the project.
How can I open the projects from the CubeL5 Package ?
Thank you for your help.
2025-01-09 12:33 AM
Try open a STM32CubeIDE project using the "File -> Import" menu.