2025-04-15 7:58 AM
Hello,
I'm stuck with Cube MX to build a M33 project for the STM32CubeMP257 Eval board STM32MP257x-EV1
I managed to run the projects in the firmware repository but I didn't find any ioc file to use.
Then, I tried to start a project with CubeMX
But it says the RCC config is wrong and I don't understand what is going on.
The flag on RCC is green but it doesn't generate RCC code for the main.c
Is it possible to find the ioc of the demo projects present in the firmware repository ?
Best regards
Stéphane Mancini
2025-04-16 1:36 AM
Hello @stephane_mancini ,
First let me thank you for posting and welcome to the ST Community.
For more investigation, I suggest that you provide your Ioc.File.
Thanks.
Mahmoud
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.