2024-07-17 12:36 AM
Hi,
I am using the latest version v1.16.0 STM32CubeIDE with stm32g071cb.
It is not possible to use ADC1_IN16 (PB12). I have created also a new project to test this condition.
Changing the sequencer disables IN16 or makes error condition.
I need PA2 -PA3 and PB12 pins (IN2-3-16 channels to ADC sampling)
Below attached screen view and the ioc file generated via STM32CubeIDE
Regards
Murat
Solved! Go to Solution.
2024-07-17 12:57 AM - edited 2024-12-02 2:11 AM
Hello @istepne
This issue has been reported in this post and it will be solved on the coming Cube Tools Releases.
Update: this issue has been solved on the STM32CubeMX V6.13.0.
Best Regards.
STTwo-32
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2024-07-17 12:57 AM - edited 2024-12-02 2:11 AM
Hello @istepne
This issue has been reported in this post and it will be solved on the coming Cube Tools Releases.
Update: this issue has been solved on the STM32CubeMX V6.13.0.
Best Regards.
STTwo-32
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.