cancel
Showing results for 
Search instead for 
Did you mean: 

ADC1_IN16 uasge

istepne
Associate III

Hi,

I am using the latest version v1.16.0 STM32CubeIDE with stm32g071cb.
It is not possible to use ADC1_IN16 (PB12). I have created also a new project  to test this condition.
Changing the sequencer disables IN16 or makes error condition.
I need PA2 -PA3 and PB12 pins (IN2-3-16 channels to ADC sampling)
Below attached screen view and the ioc file generated via STM32CubeIDE

istepne_1-1721201408556.png

Regards

Murat

 

 

 

1 ACCEPTED SOLUTION

Accepted Solutions
STTwo-32
ST Employee

Hello @istepne 

This issue has been reported in this post and it will be solved on the coming Cube Tools Releases.

Best Regards.

STTwo-32

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

View solution in original post

1 REPLY 1
STTwo-32
ST Employee

Hello @istepne 

This issue has been reported in this post and it will be solved on the coming Cube Tools Releases.

Best Regards.

STTwo-32

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.