2020-11-21 1:09 AM
i am not able to flash the image in stm32mp157c-dk2
Solved! Go to Solution.
2020-11-23 11:53 PM
Hi @MVENN.1 ,
Only the last version 2.6 is supported on Ubuntu 20.04.
And since this version the JRE is bundle inside STM32CubeProgrammer and no longer need extra JRE package.
Olivier
2020-11-24 12:00 AM
The installation PATH of STM32CubeProgrammer is not the good one as expected.
You have to install in "$HOME/STM32MPU_workspace/STM32MPU-Tools/STM32CubeProgrammer-2.5.0/" and add the binary path to path environment variable "export PATH=$HOME/STM32MPU_workspace/STM32MPU-Tools/STM32CubeProgrammer-2.5.0/bin:$PATH"
Armand
2020-11-24 12:05 AM
Hi Olivier GALLIEN (ST Employee )
Thank you for reply.
I am just installer STM32Cubeprogrammer 2.5.0 version in Ubuntu 20.04
can you please give steps to install the 2.6 version.
Thanks
2020-11-24 12:29 AM
please once check it. actually i installed everything but i did small mistake i don't know.
Thanks
2020-11-24 1:05 AM
Hi @MVENN.1 ,
Download STM32CubePrg-Lin package here : https://www.st.com/en/development-tools/stm32cubeprog.html
Olivier
2020-11-24 2:02 AM
Hi Olivier GALLIEN (ST Employee)
Thanks its working fine.
when I launch and connect the device it shows like
I installed USB port also.
2020-11-24 5:27 AM
Hi Olivier GALLIEN (ST Employee)
I can able to install and connecting is ok but when i connect the device it showing like this please once check it.
Thank
2020-11-24 5:41 AM
please check i getting this warning
2020-11-24 5:41 AM
2020-11-24 5:42 AM
When i flash the image in between connection is loss